Hello Franziskus,
In the TPS3702 datasheet Figures 5-2 and 5-3 show the temperature dependant portion of the overall accuracy and Figures 5-4 and 5-5 show the initial production tolerance. The overall 0.9% accuracy is the combination of both of these.…
Part Number: TPS3702 Hi all Would you mind if we ask TPS3702? <Question1> The datasheet shows the typical value of tpd(HL) and tpd(LH). Do you have the mininum value and maximum value of them? We guess that y ou do not test this spec in production for…
Hi Ishiwata,
Depending on the orderable part number of the TPS3702 you have will determine the behavior of the SET pin. In general setting it High or Low is dependent on your use case and design. The image below shows the OV/UV tolerance settings.
For…
Part Number: TPS3702 Other Parts Discussed in Thread: TPS3760 HI team,
My customer is looking for detection IC that can send a reset signal at below condition. They want to detect a short situation between 5V power rail and UART data trace.
I wonder if…
Part Number: TPS3702-Q1 Hi team,
I would like to confirm whether the (VIT –) and (VIT+) error is chip-driven or VDD-related? thanks
for example ,when i set Vdd=3.3V, 3.3V itself has errors maybe it is 3.2V actually , so in this situation, worst…
Part Number: TPS3702 Other Parts Discussed in Thread: TPS63070 , , TPS3840 , TPS37 I have two questions. Here's the background of the circuit I'm trying to produce.
I'm trying to make a 5V power supply, powered by 4x AA batteries, using the TPS63070…
Part Number: TPS3702-Q1 Hi Team,
A customer is asking for the minimum value of High-level output voltage (VOH) as it is not available in the datasheet
Thank you.
Regards,
Marvin
Part Number: TPS3702 Hi,
TPS3702CX10QDDCRQ1 is used by mounting 6 channels on one board. The TPS3702CX10 has a threshold of 1v.
However, when we verified the operation, there were unexpected operations with thresholds of 3.2V, 1.2V, and 4.8V.
If you have…
Part Number: TPS3702 How shall be the impact of hysteresis value interpreted? Datasheet notes hysteresis of 0.55% (min 0.3%, max. 0.8%) plus a note: of nominal trip point. What does this exactly mean?
Example: TPS3702CX33 +/-4% nominal thresholds, +/…
Part Number: TPS3702 Other Parts Discussed in Thread: TPS3703
Hi,
what is the correct way to calculate the thresholds (min / max) for undervoltage and over voltage respectively? If I read the datasheet. It is simply the nominal tolerance +/- threshold…