Part Number: TPS3702
Hi team,
In product page there is a SPICE MODEL for TPS3702CX33. Is there a model for TPS3702AX33? Also, if it is possible by changing the model of CX33, please tell me how to change it. However, when I opened the pspice model of…
Part Number: TPS3702-Q1 Other Parts Discussed in Thread: TPS3703-Q1 Hi team,
Will you release 2.8V or 3V version of TPS3702-Q1 in the future? To monitor a 2.8V or 3V voltage rail, which device do you suggest? TPS3703-Q1? Thank you.
BR,
Arie
Part Number: TPS3702 Hello,
Voltage excursions outside the ±9.9% band (worse case) in page 11 of datasheet.
Why not consider the hysteresis(0.8%) here?
Thanks in advance!
Part Number: TPS3702 Other Parts Discussed in Thread: TPS3700 , TPS3808 , , TPS3890 Can I measure 12V with the TPS3702CX33 using a voltage divider to scale 12V down to 3.3V or should I use a different device such as the TPS3700?
If I can use voltage divider…
Part Number: TPS3702 Hello I have used this IC for monitoring 1.8V rail.
Have used 10kOhm pull resistor for the output lines.
Would like to know how to calculate the power consumption and Power dissipation for the same.
Power Consumption = Icc*Vcc = 12uA…
Part Number: TPS3702 Other Parts Discussed in Thread: SN74HC244 , LMR14020 Hi team
I use TPS3702 to monitor the VCC of TMS320F28062 . I connect the UV to MCU RST pin to reset the MCU when the MCU VCC is under 2.9V and connect the OV to LMR14020 EN pin and the…
Part Number: TMS320F28377D Other Parts Discussed in Thread: TPS3702 Hi,
TMS320F28377D recommend voltages are "1.14V<VDD<1.26V" and "3.14V<VDDIO<3.47V",
Controlcard uses TPS3702CX33 and TPS3702CX12,
They monitor voltages…
Part Number: TPS3702 Other Parts Discussed in Thread: TPS3700 Hi Team
As you can see in the picture, I used 10K as the value of Rpu in my design. But in the datasheet of TPS3702, the range of IUV is 0.3mA to 10mA. so I want to ask;
1. If I used 10K…
Hi Abhishek,
Unfortunately there are no currently released similar higher accuracy TPS3702-Q1 type devices. The last option for UV would be to go with a device like TPS3703E4080DSERQ1 and use high accuracy resistors to set the adjustable threshold. For…