Hi Ross,
The PG for LP5912-Q1 is an integrated voltage supervisor (SVS). The output voltage is compared to the reference voltage. When the output voltage is above 94% of its nominal value, the pulldown FET is released after a 140 us delay. The FET will…
Part Number: TPS3700-Q1 Other Parts Discussed in Thread: TPS3702-Q1 , TPS3700 Hello,
My Customer is doing timing verification of TPS3700-Q1 and TPS3702-Q1.
They want to do an accurate value calculation.
So, Do you have bellow min & max values of each device…
Other Parts Discussed in Thread: TPS3700-Q1 , TPS3702-Q1 , TPS3700 Hello,
According to Figure 1 of TPS3700-Q1, should I use "VIT+"-"Vhys" as VIT-(min) minimum detection under voltage?
If yes, the VIT-(min) is 384mV(min). ( VIT+(min) …
Other Parts Discussed in Thread: TPS3702 Hello Sir/Madam,
TPS3702BX10-Q1 OV/UV monitor meets the accuracy requirements of our design which is in prototype phase. In its datasheet it is mentioned that this is not released version of TPS3702 and contact…
Part Number: TMS320F280049M
Hello, I'm studying the part with my customer.
Q1. I think the part doesn't have BOR. Therefore if we need the function, a reset IC like TPS3702 would be put. Correct ?
Q2. I think its control card schematic doesn…