Part Number: TPS3803-Q1 Hi team, My customer is thinking of replacing to -EP from -Q1 due to delivery issues. Is TPS3803-01-EP made using the same die as the TPS3803-01-Q1? Sincerely. Kengo.
Part Number: TPS3805H33-EP Other Parts Discussed in Thread: TPS3803 Hello,
I currently have two reset circuit designs using the TPS3803 and the TPS3805. I would like to know if since they are manufactured using the same die, since they are on the same…
Other Parts Discussed in Thread: TPS3808-EP , TPS3808 Dear Sir/Madam
The ti supervisory ic TPS3808-EP is radiation tolerant or not.???In datasheet its specified that its able to be used in aerospace and defense applications.
Part Number: TPS71501-EP Tool/software: Hello,
Please let us know the process followed for adding gold in the termination (Immersion or Plated) ? Also if any of these parts are with pre-tinned terminations ? If so, What is the process followed (Dynamic…
Part Number: TPS3803-Q1 Dear team
The customer would like to know, what different about TPS3803-01MDCKREP,TPS3803-01QDCKREP and TPS3803-01QDCKRQ1.
Could you help to recommend.
TPS3803-01-EP:
TPS3803-01MDCKREP
TPS3803-01QDCKREP
TPS3803-01-Q1…
Part Number: LM5116 Other Parts Discussed in Thread: LM5145 , , LM5164 Tool/software: Hi,
One of my customers has the following question.
The TI parts that I am using are LM5116, LM5145 and LM5162. Attached is the schematics for the supplies that…
Part Number: TPS3803 Dear Sir, good morning
I use TPS3803-01
I have battery power supply 2.5 - 4 V. I need to set a trip point 2.7 V and I'd like to add a hysteresis in TPS3803-01
QUESTION: Can I use this application (please see attach) for TPS3803…
Part Number: TPS3803 Other Parts Discussed in Thread: TPS3808 Dear Sir, please answer
I need to add a hysteresis in TPS3803-01. Power supply is 3.6 – 2.4 V. I need to set a threshold voltage 2.7 V and to add a hysteresis.
I use TPS3808 application…