Part Number: TPS3820
1. End customer test failure: The board keeps asserting reset signal after power-up, system cannot boot up.
2. Root cause localized to watchdog circuit: The internal watchdog fails to recognize WDI feed pulses, watchdog timeout…
Part Number: TPS3820 Other Parts Discussed in Thread: TPS3828 Hi,
We are using the TPS3820-33 as an external watchdog. WDI is connected directly to an MCU GPIO.
During production programming (before firmware is loaded), the GPIO state is undefined…
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820
Hello TI engineers:
How can I get the information about TPS3820's internal auto-reset oscillator, e.g. duty, cycle time ...
BestRegards
Part Number: TPS3820-Q1 Hello,
I have several questions regarding the TPS3820-50QPDBVRQ1 device. Could you please answer each question separately?
The schematic I am using is shown below; you may refer to it while answering the questions.
Q1) When…
Part Number: TPS3820-Q1 Tool/software: Hi,
Datasheet of TPS3820-33 specifys that /RESET asserts "td" (time delay) after rising of VDD
Is "td" also applied between rising of /MR and rising of /RESET?
Thank you
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 Tool/software: Dear experts,
I'm trying to work with the watchdog TPS3820-Q1 and a NXP microcontroller. The circuit is shown in the figure below:
The signal WDI_UC is a GPIO from the…
Part Number: TPS3820 Tool/software: Hi team,
customer has a application that customer feedback TPS3820 occasionally output an unexpected reset signal.
I'd like to clarify the application first. Customer use TPS3820 to reset M0 as below schematics…
Part Number: TPS3820 Tool/software: Need the following information for the part
TPS3820-33DBVR
for operating temperature -40 to 85 deg Cel
Power Dissipation(PD)(mW)
VCC to Reset Output Delay(tRD)(uS)
Reset Timeout…
Part Number: TPS3820-Q1 Other Parts Discussed in Thread: TPS3820 , SN74AUP2G34 , TPS35 Tool/software: It was not clear to me whether the transition time of the RESETn output is specified in the datasheet. I need to understand the slew rate of the RESETn…