Part Number: TPS3825-Q1 Other Parts Discussed in Thread: TL7759 , TPS3825 Dear Sir:
Regarding the TPS3825-33QDBVRQ1 RESET IC IOH & IOL issue
1. How many uA of IOL(min)?
2. How many uA of IOL(min)?
Please check to reply it asap.
Thanks
B.R…
Part Number: TPS3825-Q1 Dear Sir:
Regarding the TPS3825-33QDBVRQ1 RESET IC Schematic Review.
VCC_3V3 = 3.3V
GNSS_RST_N : Low Active to Reset GNSS IC
Please assist to review and help comment it.
Thanks a lot.
B,R
Vincent
Hi Alberto,
See my response below in green.
1) Do you think the system could work? it would be a similar function of using the TPL5110 , which I can not use because it's not P2P compatible.
Yes, I believe your idea will work. The only concern I…
Part Number: TPS3825-Q1 Other Parts Discussed in Thread: TPS3825 , TPS3824 , TPS3823 Hi Team,
It appears that the TPS3825-50QDBVRQ1 is obsolete. Can you please provide me with the closest match to this device?
Thanks!
Jared
Hi Dominik
A little strange for your situation, as I checked that default settings should be no problem for you to use USB PLAY audio.
Just double check if PPC already choose USB as audio input, also unmute SPK as below picture.
If still no sound…
Hi, Radomir,
Sorry for my late response.
The USB female port part number is 47346-0001. Molex is the manufacturer. Please find attached the AIP006G_BOM (PurePath-CMBEVM BOM) for more details.
AIP006G_BOM.xls
Please let me know if you require additional…
Hello Michael,
You can actually configure the TAS5825M in 2.1 configuration as well, we typically recommend that board over the 2.1 board.
AIP006G Schematic.pdf
https://www.ti.com/lit/ug/tiduen4/tiduen4.pdf Is the reference design documentation…
Part Number: PUREPATH-CMBEVM Hello,
I'm just getting started with the evaluation. I'd like to run 192kHz sample rate signals to test performance over the entire frequency range of the device.
A few questions -
1. I was surprised there is no technical…
Hi Jon,
You could refer below PPCMB EVM User Guidance to customize your own signal routing.
3108.Purepath Console Motherboard User Guid.pdf
Regards,
Matthew
Hi Kelvin,
1. Which is your side lasted version Purepath Console Mother board? Both F and G have external I2S interface at the similar position.
Here is the User Guide for your reference:
2. Our college will follow up HF5 and HF7 script soon…