Part Number: TPS3851 Hi.
We are using a TPS3851 connected as:
During power on when reset is deactivated and also when we stop kicking when reset is released it's not consistant: Picture below shows the reset pulse when kicks has been turned off:
…
Part Number: TPS3851 Hi team,
My customer would like to use TPS3851 in their project.
Below is the schematic, could you please help review and give some comments?
Thank you!
Regards,
Ivy
Part Number: TPS3851 Hello,
could you help check if there is any PCN NOTICE forthe part#TPS3851H33EDRBR about the Internal structure ?
Based on the x-ray, the pins of the parts are different。
any pcn? and the change will impact the function of the parts…
Part Number: TPS3851 Other Parts Discussed in Thread: TPS3430 In TPS3851G50EDRBR (5 V -operating IC) is it possible to operate as below,
VDD (Pin 1) - Connected with 5V supply.
WDO (Pin 7 ) - Connected through a pull up to 1.8V supply.
RESET (Pin 8 )-…
Part Number: TPS3851-Q1 I am creating this post as we have been having issues with the MR manual reset pin on the TPS3851-Q1 (TPS3851G30SQDRBRQ1) in our product. According to the datasheet Table 5-1 this pin is pulled up to VDD internally. However, when…
Part Number: TPS3851 Hi Team,
My customer has some question about TPS3851. Could you please give me some advice.
Customer request: Internal to CPU which should generate a board-wide hardware reset if not ticked in 10 to 20 seconds
So CWD pin is pull-high…
Part Number: TPS3851 Hi Team,
Could you please review schematic of TPS3851H33EDRBR.
Below is the schematic of TPS3851H33EDRBR, I think the circuit is ok, but I am not very sure.
Part Number: TPS3851 In TPS3851G50EDRBR (5 V -operating IC) is it possible to operate as below,
VDD (Pin 1) - Connected with 5V supply.
WDO and RESET(Pin 7 and 8 tied together) - Connected through a pull up to 1.8V supply.
Is it possible to use different…
Part Number: TPS3851 Hi Team
My customer have one question about TPS3851.
The circuit in p.1 of datasheet shows reset pin on the TPS3851 connects to reset pin on the microcontroller, and t he WDO pin of the TPS3851 is connected to the NMI of the microcontroller…