Part Number: TPS3852-Q1 Hello,
I have the following schematics of the part:
The power supply is 3.3V and I am testing with a regulated power supply the voltage monitoring of the part. When I decrease from 3.3V to 2.5V the power supply, theoretically…
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS36-Q1 , TPS3436-Q1 We have a requirement as highlighted below -
Here, the requirement is clear as separate time based & window watchdogs.
Timing is not the issue here, but the type of…
Part Number: TPS3852 Other Parts Discussed in Thread: TPS3851 Dear Teams,
My customer wants to change from TPS3851 to TPS3852. However, they found that TPS3852 actually is a window watchdog timer, while TPS3851 is an independent watchdog timer. Refer…
Part Number: TPS3852-Q1 Hi Team,
My customer find when they pull down the SET1 Pin to GND, the WDO/ still has the output, which is not matched with the following waveform.
Only when they re-start the device (power off then power on), the WDO/ can…
Part Number: TPS3852-Q1
hi team,
could you help support this problem.
VDD to 3.3V, CWD to ground via 100pF capacitance, SET1=1 If the VDD voltage remains at 3.3V, What should the WDO output waveform state when the WDI input waveform is in the tPULSE…
Part Number: TPS3852-Q1 Tool/software: Hi,
I would like to know the values of input low current (IIL), input high current (IIH), output low current (IOL), and output high current (IOH) for TPS3852-Q1.
Thanks & regards
Priyanka S P
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3852 , Hello,
I received the TPS3852G33DRBR today and tested it on our circuit, but it didn’t work as expected.
The WDO works as expected if WDI stays high. I see the pulldowns every ~84seconds…
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3890-Q1 , TPS3852 , TPS3890 Hi Expert,
Our customer uses TPS3852-q1 in their project. But they don't use TPS3890-q1, which is suggested in datasheet as below. The SET1 pin is directly tied…
Part Number: TPS3852 My customer is having some manufacturing issues with placing vias underneath the body of the part and is asking whether the recommended vias could be either eliminated or moved away outside the perimeter of the footprint.
Is the…