Part Number: TPS389006-Q1
Tool/software:
Hi Everyone,
I am using two TPS38900603NRTERQ1 which share an NIRQ Line with a LED and a 560R Resistor pulled to a 3.3V Rail.
There should be a maximum current of 2.7mA flowing. (3.3V - 1.75V LEd)/560R (Assuming…
Part Number: TPS389006-Q1 Other Parts Discussed in Thread: TPS389387EVM , Hello,
I am using the TPS389006-Q1 with the TPS389387EVM Joint Evaluation Module and I have the following flag error inside the following registers:
INT_VENDOR (0x24): 7F TEST_INFO…
Part Number: TPS389006-Q1 Other Parts Discussed in Thread: TPS389006 , Tool/software: Hi BU team
What are the differences when tps389006-Q1 pin9 nSync is set high and low? Is it ok that connected sync pin between multiple tps389006?
It is not clear in…
Part Number: TPS389006-Q1 Other Parts Discussed in Thread: TPS389006 Hi,
the Fusion Digital power Device Gui detects the TPS389006 as TPS389004 and therefore only 4 Channels are displayed.
Is there a new software version available which supports 6 channels…
Part Number: TPS389006-Q1 Hello I am a software engineer,
I observed a voltage drop when connecting power supply to a monitor PIN of TPS389006-Q1.
Does the monitor have low input impedance ?
How can I avoid this issue ?
Best regards,
Tom LEVISSE
Part Number: TPS389006-Q1 Hi TI,
Can we use 47K ohm resistor for I2C addr 0x34?
On datasheet, TI recommend 47.5kOhm but I think 47Kohm can use as well.
Because it is close to 47.5K rather than 37.4K and 58K.
Best regards,
Part Number: TPS389006-Q1 Hello expert,
Are there some possibility to cause ACT wave from 1 to 0?
Situation 1: ACT is pull up to VVDD_3V3 through R8, As shown in the following picture, ACT is driven to 0 about 1.5ms and than turn back to 1.
Situation…
Part Number: TPS389006-Q1 Dear TI Team,
I just wanted to ask whether it is possible to override all settings with custom values (UV_HF / OV_HF, Scaling...) via I2C and save them to the device.
Thank you very much.
Kind regards Moritz
Part Number: TPS389006-Q1 Other Parts Discussed in Thread: TPS389006 Hello Power Team,
I have a few questions about the BIST:
1. How is the BIST guaranteed to be running at power up when it needs to be configured first? The datasheet implies that this…