Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3422 , TPS3899 Tool/software: Hello, We are considering TPS3899-Q1 for our design. Our use case conditions are as follows: 1. If the push-button connected to sense pin is pressed for a duration…
Part Number: TPS3899-Q1 Hi Team,
In our circuit design featuring the Voltage Supervisor ( TPS3899DL31DSERQ1 ), we've set the undervoltage threshold to 3.1V. However, during RF data transmission, the voltage drops below this threshold, triggering the…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hello,
Earlier we are using LTC2954CTS8-1#TRMPBF, Now we are planning to replace with TPS3899DL01DSERQ1.
Could you please review the connection of power ON/OFF control IC TPS3899DL01DSERQ1…
Part Number: TPS3899-Q1 Are there minimum and maximum values for the Negative-going input threshold for adjustable sense threshold TPS3899DL01DSERQ1?
The datasheet only specifies a typical value, which does not support calculation of upper and lower…
Part Number: TPS3899-Q1 Other Parts Discussed in Thread: TPS3899 Hi,
In the datasheet of TPS3899-Q1, I don't understand Figure 7-3:
1. What is the meaning of "VDD=SENSE", is the two pins connect together?
2. Since the width of positive pulse on…
Part Number: TPS3899-Q1 Hello,
My customer considers using the TPS3899DL01DSERQ1 with the follwoing conditions.
How does RESET# work when V1 power is shorted to GND or V1 power is not supplied due to a disconnection?
Thank you.
JH
Part Number: TPS3803-Q1 Other Parts Discussed in Thread: TPS3808E-Q1 , TPS3890-Q1 , TPS3899-Q1 Goodmornig,
I shall power supplies the device TPS3803-01QDCKRQ1 at 1.8V.
On my schematic, the SENSE pin can go up to 6V. I would like to know if that pin…
Part Number: TPS3840-Q1 Other Parts Discussed in Thread: TPS3899-Q1 Hello TI team,
Please help to clarify why the test result of reset time is lower than calculation result a lot.
The IC we used is TPS3840DL29-Q1 (open drain and V_IT-=2.9V). I connected…
Part Number: TPS3899 Other Parts Discussed in Thread: , TPS3842 Hi
I am caculate the range of the tD-SENSE (min) or tD (min) and the tD-SENSE (max) or tD (max) .
I can not find the Rct(min) Rct(max) and tD(no cap,min) in the datasheet.
Only typical…