Part Number: TPS40050-Q1 Other Parts Discussed in Thread: TPS40054 , , TPS40057 , TPS40050 Hi
We were testing the TPS40050-Q1 and comparing with the TPS40054/TPS40057 and everything is pretty similar. We have a doubt about switching frequency. Basically…
Part Number: TPS40050 Hi.
What is the difference between TPS40050 and TPS40050-Q1 beside the latter is AEC Qualified and temperature range is -40 to +125. Is there a difference in performance calculation? Can I replace a TPS40050-Q1 with a TPS40050 without…
Part Number: TPS40050-Q1 Other Parts Discussed in Thread: LM25148 Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with " MAX20098 " ?
1. It seem that TPS40050-Q1 can fight with MAX20098…
Part Number: TPS40050 Other Parts Discussed in Thread: TPS40055 , TPS40057 , LM25116 , LM25117 , LM25145 , LM5145
Describe : RKFF = 62K & RA = 430K that SMPS can normal work (Turn on point at 10V when ambient = 25 deg C)
issue : The turn on point (UVLO…
Part Number: TPS53015 Other Parts Discussed in Thread: CSD87350Q5D , , SYNC-BUCK-FET-LOSS-CALC , TPS40050 , LM3150 Hi TI,
I'm seeking for alternate part for the switching controller TPS53015DGS , I had designed the part for below mentioned configuration…
Hello Chester,
I interpret the statement as TPS40051 is suitable for load sharing application, TPS40050 is not.
I will need to confirm, but I do not see anything in the datasheet that tells me TPS40057 is unsuitable for load sharing.
Part Number: UCC39002 Other Parts Discussed in Thread: TPS40050 , UCC29002 , LM25145 , TPS2412 Hello
We have a request to implement 1+1 redundent &power sharing based general industry Power supply.
The general industry Power Supply is 220V/100V AC input…
Part Number: LM5119 Other Parts Discussed in Thread: TPS40050 , UCC39002 Hi Expert,
The customer would like to consider the LM5119 into their redundant PSU.
Condition:
PSU1 12V from LM5119 ( Interleaved Single Output)
PSU2 12V from LM5119 ( Interleaved Single…
k.kral,
This is possible. Just use Sync I/O as you described. Here are a few app notes showing current-sharing with other TI parts:
TPS54620 in parallel operation and Load-Sharing TPS40050
-Sam