Other Parts Discussed in Thread: SWITCHERPRO , TPS40056 HI there,
my customer has looked both in switcherpro and TINA and has been unable to find the spice model for TPS40056.
Please advise where to find it.
Thanks,
Amy
Other Parts Discussed in Thread: TPS40056 , LM25117 Hi, We are looking for a Buck Controller device where the ouput voltage reference is settable by a voltage, I2C or SPI interface. The device needs to meet the following specifications:
- Input voltage up…
Other Parts Discussed in Thread: TPS53315 Hi,
I'm looking for a buck converter that is capable off sinking and sourcing. The output needs to be adjustable so the controller needs preferable an external reference.
Input: 10V -> 14V Output: 1V -> 5V…
David,
If I am understanding your requirement right, you would like a 2-state non-isolated DC/DC Converter capable of sourcing current at a 15V output and sinking current at a 2V output?
If that is correct, there are several ways to do this. One…
Other Parts Discussed in Thread: TPS40056 A customer is looking for a DDR3 VTT termination.
Vin = 12V
Iout = 8A
Do we have an integrated device that can do thie?