Other Parts Discussed in Thread: TPS40061 , TPS40060 Hi,
i have some questions about the different between TPS40060 and TPS40061,
1. what is two quardrant operation and one quardrant operation?
2. what does output current sink and source mean, and what…
Other Parts Discussed in Thread: TPS40060EVM I want to teach the questions.
We test under the following conditions
But output voltage is dropout.(12Vout→5Vout)
1. Output possible? Under the following conditions:
Vin 12.5V
Vout12V±10%
Iout:(min…
Part Number: TPS40061 Other Parts Discussed in Thread: TPS40060 , LM25145 , LM5146 , LM5145 Hi,
TPS40061 seems have no webench design tool, does it have any excel desing tool or only can step by step design by datasheet?
or can follow the TPS40060 EVM design…
Other Parts Discussed in Thread: LM25145 , LM5146 , LM5145 , TPS40060 , LM5116 , LM25117 , LM62460 , LM61460 Hello.
I started to design a 5V/6A syncrounous buck converter. Vin = 10 - 28 Vdc. Requirements: efficiency > 93 %, board area < 700 mm2.
I used WEBENCH…
Other Parts Discussed in Thread: TPS40060 , LM5085 , TPS54360 , TPS54260 Hi! I am developing buck converter, which is able to operate at true 100% duty cycle. The input voltage can change from 10 to 34 Volts, but ouptut voltage is 12V (or equal to input voltage…
Other Parts Discussed in Thread: TPS51216 , TPS40060 , TPS51916 I am choosing power regulator with these parameters:
Vin=28V, Vout=1.2V, Iout=5A.
2 results come out. TPS40060 ( Wide Input (10V-55V) up to 1 MHz Frequency Synchronous Buck Controller, source…
Other Parts Discussed in Thread: TPS40060 , TPS40061 Good Day to all gurus , We are in the process of developing a dc to dc convertor for an automobile application .
We are facing some issues like the following ;
The chip we use is TPS40060;
Basic Spec…
Hi Robin,
TI does support TPS40060. You can obtains answers on this part in the
"Non-Isolated DC/DC" forum. However, TI has not added the TPS40060 into
SwitcherPro, which is our SMPS design tool. For people who are not
familiar with SMPS design…
Other Parts Discussed in Thread: TPS40060 Hi,
We are designing an application need to step down voltage from 48V input to 12V output with current up to 4A. Whether TPS40060 is a choice? Otherwise, recommend us with some IC met this requirements.
Tha…
Other Parts Discussed in Thread: TPS40060 , TPS40061 I recieved this from a customer (Customer Information and schematic removed)
Please find our detailed spec below
Basic Spec:
Vin (min) = 18V
Vin (max) = 36V
Vout = 14 V ;
I out = 10 A;
Fsw =…