Hi Anish,
Currently we do not have the TINA model for TPS40056. However, we do have TINA-TI models and SwitcherPro support for several parts in this family which are listed below. Can you customer use any of these models instead?
TPS40055: http://www.ti…
Other Parts Discussed in Thread: TPS40050 , TPS40060 , TPS40170 Hello,
I am a engineer from Hyundai Motors. and I am working in converter department.
But we have some problems to improve our DC-DC converter.
We now use TPS40060 that is not for automotive…
Other Parts Discussed in Thread: TPS40061 , TPS40060 We've found an unusual shutdown problem in a few TPS40061 devices, about 7 or 8 so far. The faulty devices would appear to exhibit thermal shutdown at a case temperature of 60C to 65C. As the case…
The TPS40050 and TPS40060 controllers are source only (diode emulation) versions of the TPS40051 and TPS40061 controllers.
The TPS40051 isn't modeled in Switcher Pro because it has been Not Recommended for New Designs prior to its integration into the…
The TPS40200 controller will not support a 60V surge voltage. The absolute maximum voltage is 52V, anything higher could result in IC damage.
The TPS40060/61 is a similar part, though allowing synchronous rectification. The TPS40060/61 could drive…
Other Parts Discussed in Thread: TPS5450 , LMZ13610 , LM25117
I am finding the following specs.
Vin (nom) (V) = 28
Vout1 (V) = 2.5
Iout1 (A) = 10
TPS40060 and TPS40170 come out. When I read the datasheet. There is no mention of the Iout…
Other Parts Discussed in Thread: TPS40060 , SWITCHERPRO , TPS40061 , TPS40200 Hi, all , i wanted to know how to add a new device e.g "TPS40060" in switcher pro that is not currenly a part of device list
Regards
Ahmed
Other Parts Discussed in Thread: TPS40060 HI
i m a student.i have some problem related with power supply.i m using tps40060 buck regulator for vin 48vdc ,ouput 5vdc @ 6A.in example surge current is given for 3.3vdc output .but how can i calculate with…
Other Parts Discussed in Thread: TPS40060 hi all
i am using tps40060 for 48vdc input and need 5vdc output @ 6A current .in data sheet give example 48 to 3.3v @ 4A .actuly i am facing problems regarding calculation .please its very arrgent any one can change…
Ankur,
Here are a couple of parts you should take a look at. I've also attached a reference design for a lower power system. The reference design uses the TPS40200.
TPA40057 – VOUT = 35V and Iout = 20 A Buck Controller http://focus.ti.com/docs…