Other Parts Discussed in Thread: TPS40061 I am developing a design using the TPS40061 part and following the datasheet.
I am trying to determine the values for Rt and Rkff. Using equation 2 and 3 from the datasheet, I see the relationship between these…
Other Parts Discussed in Thread: TPS40061 Hi,
I am using TPS40061 as indicated in slvr235.pdf and see that it is burned frequently . Has anybody meet such kind of burning or problems?
I give the rated values.
Other Parts Discussed in Thread: TPS40061 , TPS40060 Hi all,
We are using TPS40061 in our design. I looked at the datasheet but there is no mention of the maximum output current. However in the specification page for the part the maximum current is set…
Other Parts Discussed in Thread: TPS40061 , TPS40060 , SWITCHERPRO , TPS40200 Hello All, I wanna know whether tps40060 or tps40061 devices are included in TPS40k designer Software (Any version) or not? I hv searched in Switcher Pro these two devices are not…
Part Number: UCC21520 Other Parts Discussed in Thread: TINA-TI , TPS40055 , TPS40057 , TPS40061 Hello Texas Instrument Forum,
I am using TINA-TI to simulate my DC/DC Synchronous Buck Converter from 500V down to 200V. The purpose is to use SiC MOSFETs, and…
Part Number: LM5085 Other Parts Discussed in Thread: TPS40060 , LM5088 , , TPS40061 , LM5117 I'm doing the research to implement a DC-DC CC+CV to charge a 10s4p pack, at 0.5C = 5A, from a 48VDC supply.
I'm VERY newbie at power electronics.
Is it enough…
Other Parts Discussed in Thread: TPS40060 , LM3488 , LM5022 , TPS40061 Looking for a Step up converter.
Input = 9V to 16V
Output = 24V, 2A.
Require suggested parts.
Regards,
Murugavel.A.N
Other Parts Discussed in Thread: TPS40061 , TPS40060 , TPS40052 Dear community, in a circuit (DCDC converter) i found a ti ic which i cant find informations about it. its written 40062 02t a1506 on it next to the ti logo. i found the TPS40061 datasheet,…
Hi Amy,
Currently we do not have the TINA model for TPS40056 . However, we do have TINA-TI models and SwitcherPro support for several parts in this family which are listed below. Can your customer use any of these models instead?
TPS40055 : http://www.ti…
Hi Anish,
Currently we do not have the TINA model for TPS40056. However, we do have TINA-TI models and SwitcherPro support for several parts in this family which are listed below. Can you customer use any of these models instead?
TPS40055: http://www.ti…