Part Number: TPS40170-Q1 Other Parts Discussed in Thread: LM5141-Q1 , hi
If same Load condition: LM5141-Q1 & TPS40170-Q1, which one performance is better?
Part Number: TPS40170-Q1 Other Parts Discussed in Thread: TPS40170 , LM5145 Hello team,
My customer have some problems with high frequency noise.
They used 1200pF of C21(compensation capacitor) because TI EVM used 820pF.
Is it okay to compensate the circuit…
Part Number: TPS40170-Q1 Hello all,
I am designing a customized board for my application. My board works on 12V and it requires 15A output current. I need to step down from 48V to 12V for my application. So, I am using TPS40170-Q1 for this application…
Part Number: TPS40170-Q1 Other Parts Discussed in Thread: TPS40170 , LM5141 Hello,
I'd like to know if TI have plan to create wettable flank package of the ICs list below, thanks.
1. TPS40170QRGYRQ1
2. TPS62067QDSGRQ1
3. TPS73501QDRBRQ1
4. TPS54618QRTER…
Part Number: TPS40170-Q1 Hi,
I am using TPS40170-Q1 IC as a dc-dc converter for my application.
My requirements:
48V input
12V output
12A max current
I didn't get the output initially when I gave the input and after some time the output capacitor has…
Part Number: TPS40170-Q1 Hi,
My customer is using TPS40170-Q1 for display in car panel, but found the voltage ripple is abnormal, I have uploaded the schematic and layout files. Could you please help us on this issue? Thanks.
YDB23HP000FF-MP4-B01-20180917…
Part Number: TPS40170-Q1 Other Parts Discussed in Thread: TPS40170 Tool/software: WEBENCH® Design Tools Is it possible to download WEBENCH Power Designer Tool from TI website?
Other Parts Discussed in Thread: TPS40170-Q1 Hello,
If I want to use two TPS40170-Q1 as below, Do I only need to set M/S pin as one is Master & the other is Slave and connect Sync pins ?
Or Need more setting?
Regards,
Nicky
Part Number: TPS40170-Q1 Other Parts Discussed in Thread: TPS40170 , TPS28225-Q1 What is driving the 20A max limit posted on the TPS40170 product page? Looking to use this chip for 25~30A and the only thing that seems to me to limit the max output current…