Part Number: TPS40305 Hi,
We are using TPS40305 to convert 8-16V (VIN) to 4.5V (@9A) Vout.
This power supply is becoming main culprit in the PTCRB certification (not able to reach to the limitations for TIS). As soon as we remove this supply from equation…
Part Number: TPS40305
Hi
I use the evm sample and design my own board, but I have issue with output voltage which does not stabilize after input transient voltage or current. you can see in below graph the voltage stay off until high current or transient…
Other Parts Discussed in Thread: TPS40305 art Number: TPS40305
Hi
I am using TPS40305 in my circuit and the output ripple does not match my calculation. My ripple is around 75mV which is a lot higher than 35mv calculated. What could be the reason, the only…
Part Number: TPS40305 Our product is failing in the 200MHz-1GHz FCC EMI Testing.
After the debugging we have identified that we TPS40305 is generating that noise specifically Q7 & Q8.
Kindly find the result of EMI test.
Kindly find the layout screenshot…
Part Number: TPS40305 Team,
Can you please help my customer with an implementation of TPS40305:
The circuit is not regulating correctly under load. I see your WEBENCH tool for the device but it is very limited since my MOSFETs and Inductor are not in…
Part Number: TPS40305 Other Parts Discussed in Thread: TPS40303 , TPS62130 , TPS82130 Hi -
I have a design that uses the TPS40305 configured in a feedback regulated constant current configuration to deliver 26A to an LED. This design has been adapted in…
Part Number: TPS40305 Hi team,
We have some issues using TPS40305. Our condition is Vin = 12V / Vout = 6V / Iout = 1.5A.
After calculation, I set Rs = 3kohm and our MOSFET is using https://www.infineon.com/dgdl/irfs4615pbf.pdf?fileId=5546d462533600a4…
Part Number: TPS40305 Hi,
I am using TPS40305DRCR switcher IC to generate 3.3V from 5V input. It is designed to generate 3.3V with 9A load. The switching frequency is 1.2 MHz. When I connect an external load of 1A or more, I am receiving ripples at input…
Other Parts Discussed in Thread: TPS40305 , PSPICE-FOR-TI Hi all,
I am getting the following error message when trying to simulate a PSpice circuit using the TPS40305 part from the library in the program:
ERROR(ORPSIM-15461): Incorrect number of interface…
Part Number: TPS40305 Hi TI Team,
We are using TPS40305 switcher with 5V input and 3.3V, 9A output. We are facing issue in pre-compliance test (FCC Part 15B). We are getting out of limit 160MHz broadband noise. Can you please help on reducing this broadband…