Part Number: TPS40345
Tool/software:
Hi, TI
How to select input capacitors for a buck converter slyt670 How to select input capacitors for a buck converter
From slyt670, we know the calculation of Cin(min) is the Equation (1) with D = Vout / Vin.
But…
Part Number: TPS40345
Tool/software:
Hello,
In my design , I use the TPS40345DRCR to output power on a rail. I need to adjust (lower) VREF at times to adjust the output set point:
https://www.ti.com/lit/ds/symlink/tps40345.pdf?ts=1717945785633&ref_url…
Part Number: TPS40345 Hello,
My customer is using the TPS40345 as FPGA core power supply.
Below is the output ripple capture image. The measured output ripple characteristic is significantly worse than guided by the datasheet.
Below are the customer design…
Part Number: TPS40345 Other Parts Discussed in Thread: LM10011 , LM10010 Hi,
I would like to use a TPS40345 buck controller to deliver between 1.12V (5W) and 1.5V (9W) to a 0.6 ohm load.
The buck's high side is connected to a 3.7V battery, the TPS 40345…
Part Number: TPS40345 I want to simulate ripple caused by load fluctuation.
I want to do a simulation that changes the load like 5V/5A -> 5V/8A -> 5V/5A
(Image USB type c load)
Part Number: TPS40345 Other Parts Discussed in Thread: TPS40303 Not able to get the AC model for DCDC converter designed using TPS40345DRCR in Webench power designer tool. When exported to TINA TI, every time only transient model gets exported.
The website…
Part Number: TPS40345 Hi
I would like to use the TPS40345 in a new design ,
the new design is a high power LED driver 7V@10A and 4.5V@10A
I plan to test this design using the TPS40345EVM-353 with some modification to the feedback resistor
Can you please…
Part Number: TPS40345 Good afternoon,
I made a power supply with TPS40345 using webench designer.
The features are:
Vin = 3,3V;
Vout = 0,85V;
Iout = 12A.
I assembled the firsts ten machine and two of these have the power supply that doesn't work.…
Part Number: TPS40345 Hello:
Do you have TPS4034 series design tools, preferably Excel format for loop calculation.
Best Regards
Leon
文晔集团
广东省深圳市南山区高新中三道 9 号环球数码大厦 12 楼
Mobile:(86)159 8985 2994
Tel:(86)755-26743880 Ext:6643
Fax:(86)755-26743990
Part Number: TPS40345 Other Parts Discussed in Thread: TPS40305 , The TPS40345 has a recommended operating condition down to -20C. The TPS40305 has recommended operating conditions down to -40C. The max ratings for both junctions are -40C.
Will the TPS40345…