Part Number: TPS43331-Q1 Hi team,
Description: We are encountering an initialization issue with the TPS43331-Q1 . The I2C register write fails frequently on the first attempt , but succeeds upon re-trying.
On our hardware platform, the MCU's I2C…
Part Number: TPS43331-Q1 Other Parts Discussed in Thread: TPS65313-Q1 Hi team,
My customer wants to know if TPS43331-Q1 has ASIL-B verification? And do we have other devices have ASIL-B verification?
Thanks a lot.
Regards,
Cathy
Part Number: TPS43331-Q1 Hi team,
I see from the Datasheet that EN is only to enable and control BUCK1, right?
In addition, the I2C bus can control the on and off of which power supplies?
Part Number: TPS43331-Q1 Greetings,
I want to design a power circuit in my solution.
Parameters is below.
DC/DC converter
Input 24v
Power consumption about 90w
Output 3.3v ,1.8v, ±2.5v
Output via interface to supply 12 channels,
Each channel…
Part Number: TPS43331-Q1 [ TPS43331-Q1 ] Datasheet Change Related Queries
(I post here instead of Automotive forum, because it's now in read only.) Hi, I have a customer who has used TPS43331-Q1 for their project. It seems the datasheet has been update…
Part Number: TPS43331-Q1 Hi Team,
I'd like to know the maximum and minimum duty cycle.
Because in my customer's system, the input is 9-16V and the output is 1.8V for a DC/DC. Is there any potential issue for this small duty cycle application?
…
Hi Obinna,
Thanks for providing the information! Here are the options for replacement:
From our internal cross reference tool, LMZ36002RVQT and LMZM23601 seems to be good replacements for MAXM17575ALI# and MAXM15064AMB+T respectively.
…
Part Number: TPS43351-Q1 Other Parts Discussed in Thread: TPS43331-Q1 , Hi All,
I'm designing the power supply of a Jacinto6-based board and I'm using the TPS43331-Q1 as a first-stage regulator to provide 3V3 and 5V0 to my circuit. Unfortunately, after…