Part Number: TPS50601-SP Hello,
In the datasheet, you request a 10k pull-down resistor for synchronization with an external clock. Is it ok to use a resistor of lower value (e.g. 1k) ? My external clock will start with a weak pull-up of 10k during 50ms…
Part Number: TPS50601-SP Hello, I am wondering if there is a spice model for the TPS50601-SP. I know there are transient and average models but I'm not sure that will simulate the same part behavior. Thank you for your help.
Part Number: TPS50601-SP Greetings,
A customer need Thermal Resistance from junction to case (top side) of TPS50601-SP.
P/N: 5962R1022101VSC package CFP (HKH) | 20
do you have this info?
Thank u in advance.
Regards,
Part Number: TPS50601-SP The TPS50601-SP datasheet has the typical and maximum value for the minimum on time but only a typical value for the minimum off time. Can it be assumed that percentage tolerance of the minimum off time is the same as the percentage…
Part Number: TPS50601-SP Bode plot seems to give proper results at around 115KHz but once i reach lower frequencies around 104KHz there is a phase wrap and an unexpected peak on the gain. my input voltage is 3.351V and output current is 0.894A. my switching…
Part Number: TPS50601-SP Hi Space team,
I have a question regarding the TPS50601-SP (non-A version).
Can you guys confirm two aspects of the package:
The thermal pad needs to be connected externally to PGND? I see footnote #1: "Thermal pad (analog ground…
Part Number: TPS50601-SP I would like to evaluate the subject-mentioned part and would like to put a similar non-rad hard, less expensive, non-flatpack part on my prototype board. Is there something very similar to it?
Part Number: TPS50601-SP Hello team,
Hope you are doing well and staying safe. Would you mind commenting on below customer question:
It is EAR Controlled, can your team restrict access to it appropriately?
Regards,
Randhir
Hi Brent,
I apologize for the delay. As this data is not typically shared with customers, it is taking some time to process. This data is analyzed when collected to derive electrical specifications that encompass aging and then the data is archived. We…