Part Number: TPS51120 Hello,
We are encountering a regulation issue with the TPS51120 converter used in our system and we can't find why.
Context:
Component: TPS51120
Schematic: almost identical to the reference schematic in the datasheet (same…
Part Number: TPS51120 Tool/software: Hi,
We use the TPS51120RHB for the Vcore power supplier, and now we have below issue:
1. EN1 and EN2 are connected together, and set the EN1 and EN2 voltage is about 2.5V, the Vout1=3.3V and Vout2=5V, the PG1 voltage…
Part Number: TPS51120 Tool/software: Hi,
We use the TPS51120 for the 5V/3.3V buck design, and now, we find the 5V output i nductive howling when we set the light-load( the switching frequency is only less then 5KHz),
and we add the load that the Inductive…
Part Number: TPS51120 When I add a 10UF/50V MLCC to the MOSFET 24V voltage input Line
Controller Is not working
Please Check Something wrong in my Schematic
Part Number: TPS51120 Hi team,
Could you provide the SS time equation including the external capacitance (Css) and share design considerations for the adjustable soft-start setting? Thanks!
Thanks for your support!
Best regards,
Sam Ting
Part Number: TPS51120TPS51120.pdf
Hi,
I am using TPS51120 for 3.3V and 5V generation, I tried both D-cap and current sense mode but, In my whole circuitry Just the VREG3,VREG5 and VREF2 is working none of the other part is working .the DRV pins are…
Part Number: TPS51120 Hi Sir,
Our customer response the TPS51120 have PWM Double pluse issue as below,
We have cut-output not loading affect, we have try to short COMP2 to VFB2 not improve.
How can we improve this problem?
Part Number: TPS51120 Maybe I made the wrong choice of development tools / software, change it and ask again.
(I have the same question here. -> e2e.ti.com/.../835739)
===================
I am considering a MOSFET controlled by TPS51120. Are there…