Part Number: TPS51200A-Q1 Tool/software: We are using TPS51200AQDRCTQ1.
I would like to know if the PG, power good pin, is not used, can this pin (4) be left floating?
There is no functional usage of this pin in our design.
Thank you,
David
Hi Tamas,
Sorry for the slow response. Here is the feedback I received today from the PE team:
PPAP20231227-028858 is a level 3 PPAP which included a PCN letter for an unimplemented change. If more information on the PCN is required, please submit a separate…
Part Number: TPS51200A-Q1 In section 6.1 Absolute Maximum Ratings, the datasheet lists the max operating junction temperature as 150°C. However, section 10.3 Thermal Considerations, equation 4 states that the max thermal junction temperature is 125C.…
Part Number: TPS51200A-Q1 Hi Team,
We are using the TPS51200A-Q1 Sink/Source DDR Termination Regulator, part in our Layout Board file. I had attached the images of the Board file and Schematics. Please review the layout and share your feedback with us…
Part Number: TPS51200A-Q1 Dear all,
Could you teach about the difference of these devices?
I checked TPS51200A-Q1 datasheet and found 'Extended Reliability Testing'.
Is this test added to A version from non-A? Could you explain the detail of…
Part Number: TPS51200-EP Other Parts Discussed in Thread: TPS51200-Q1 , TPS51200 , , TPS51200A-Q1 Hello,
We plan to qualify the TPS51200-EP with for our applications. However, due to components shortage, we may qualify another part (TPS51200, TPS51200-Q1…
Part Number: TPS51200A-Q1 Other Parts Discussed in Thread: TPS51200 , Hi Team,
There is a good new that customer searching TI solution for NCV51400MNTXG replacement !
Please help recommend corresponding IC ! THX
https://www.mouser.com/datasheet/2/308/1/NCP51400_D…
Part Number: TPS51200A-Q1 Hi Team,
May I know the Efficiency Value/Range for TPS51200A-Q1, for the following condition
Input Voltage : VLDOIN = 1.5V ; VIN = 3.3V ; REFIN = 0.75V
Output Voltage : VO = 0.75V ; REFOUT = 0.75V
Output Sink/source Current = 0…
Part Number: TPS51200A-Q1 Hi
Attached is the thermal imaging video of two different TPS51200A-Q1 on a sample
There is a temperature issue on TPS51200A-Q1, and the temperature will rise to 42 degrees after power on.
A new TPS51200A-Q1 has been replaced…