Part Number: TPS51206
Hi, TI Support Team
A request for circuit and layout review for the following parts has been received from a customer.
Part name: TPS51206DSQR
Please reply after reviewing the attachments below.
Thanks.
Regards,
MJ
Part Number: TPS51206 Hi Team,
My customer need to asses abnormal conditions when they use new device.
Do you have Pin FMEA document of TPS51206?
It will pretty helpful to fill their abnormal condition list spread sheet.
Regards,
Takashi Onawa
Part Number: TPS51206 Other Parts Discussed in Thread: TPS51200 , TPS51200-EP , , TPS51116 , TPS51200A-Q1 Hi.
I am doing a crossreference my customer and they are looking for alternatives to the TPS51206DSQR (it doesn't have to be pin2pin). Please assist with…
Part Number: TPS51206 Hi Team,
According to the datasheet, Figure 23, VDD => VLDOIN,VDDQSNS for power up and VLDOIN,VDDQSNS => VDD for shut down sequence are recommended.
Could you tell me the risk under following sequences? Do you think device might…
Part Number: TPS51206 Hi All,
The customer is using the TPS51206 for DDR solution, and their voltage level of S3/S5 is only 1.8V.
So they are worried about this part because the minimum VLH(S3 and S5 high-level voltage) is also 1.8V.
Do you have any…
Part Number: TPS51206 Dear Team,
In one of the project, we are facing below issue in DDR termination supply.
Board 1 - VDDR_REF = 13.7 mV VDDR_VTT = 0 V Board 2 - VDDR_REF = 0.677 V (As expected) VDDR_VTT = Pulsed waveform as below,
Impedance values of IC…
Part Number: TPS51206 Hi team
Please let me confirm the definition of V_VTT & V_VTTREF.
- Will V_VTT be varied depending on VDDQSNS? And is the tolerance within V_VTTTOL?
- Will V_VTTREF be varied depending on VDDQSNS? And is the tolerance within V_VTTREFTOL…
Part Number: TPS51206 Hi team,
My customer is using the TPS51206 now, the structure is below. Whether the structure has additional issues? Real current is very small which is only 1A. Thanks.
Part Number: TPS51206 Other Parts Discussed in Thread: TPS568215 , TPS65296 , TPS51200 Hello team,
We have received inquiries from customers regarding the power supply of LPDDR4. It seems that they are in a hurry, so I would appreciate your feedback.
They…