Part Number: TPS51220 Hi
My customer has a question about the TPS51220 inductor temperature is higher
The following are the application conditions and test results
vin=19v
vout=12v (Ch2)
Iout=0.1A
L=4.7u (DCR30m ohm)
When the output current is 0.1A and…
Part Number: TPS51220 Tool/software: WEBENCH® Design Tools Hi Sir,
Can TPS51220 output 12V while input voltage is 12V?
And, please provide the WEBENCH ® Tool for me, thanks!
email:lsb@apuqi.com
Part Number: TPS51220 Other Parts Discussed in Thread: BQ25713
Hello,
I am currently using the TPS51220 as a DCDC on my system, generating 12V and 5V from a 19.5V source. I am seeing issues once I start drawing current from the TPS51220. Below…
Part Number: TPS51220 Hello Sir,
I want to confirm is it ok for 24Vin to dual 12V@17A and 12V@8A ?
Is there design tool for external components ?
Many thanks !
Part Number: TPS51220
Team,
I am trying to validate the TPS51220 which I plan to add to my EVM. I need the device to output 12V and 5V. I cannot get the EVM to output 12V on either channel. For VOUT2, I changed the R21 to a value of 297k ohm, and left…
Part Number: TPS51220 Hi team,
Let me clarify one terminology.
Equation (11), (12) shows Vdroop.
Does it mean voltage droop of load transient performance?
I look forward to hearing back from you.
Best regards,
Shota Mago
Part Number: TPS51220 Dear Sir,
I am Alec Chen, FAE form WT located in Taiwan.Our Customer Ennoconn RD is asking us to provide the power consumption for the pin as below form TPS51220 shown as below(request form their end-customer )
VBST PIN RES
CSP…
Part Number: TPS51220 Hi, Team
We have a question need you help in TPS51220,
We want to change Vo to 4.25V,
Is there any concern if we change V5SW(Pin.2) from 5V to 4.25V?