Part Number: TPS51916 Hello TI Support Team, I am using the TPS51916 in a DDR4 application (1.2V) in DCAP-2 mode with tracking discharge - Mode 0 (using 1kOhm resistor at R7 in schematic photo below). Targeting 6.5A as my limit of the output current.
…
Part Number: TPS51916 Hi Team,
My customer is working on a DDR3L power supply design that will use the TPS51916.
We have come up with some questions:
They have been mostly using Webench as a basis for the design, and had a question on the implementation…
Part Number: TPS51916 Hello TI Support Team and Community,
I am working in the standard Cadence PSpice, and not the PSpice for TI variant. There appears to be an issue with the bias point in my schematic and possibly an issue with the model. The VREF voltage…
Part Number: TPS51916
Good day Colleagues,
My customer is using the TPS51916 for DDR4 and likes this part.
Now he got RDIMM memory size increased and asks if the part can supply up to 24A of output current.
He says Webench has 20A of output current limitation…
Part Number: TPS51916 Hi Team,
When the IC was powered on, the Ivtt source current was 5.6A peak inrush current. (The width of the peak is about 5us.)
The source current limit is typ.3A, but the current is larger than that.
Isn't it assumed that the…
Part Number: TPS51916 Hi,
I'm using TP51916 on a new design with DDR3.
At startup, PGOOD is pulsing high, 1.2ms, then goes low as captured below.
As PGOOD is controling the board reset, the complete board is held in reset.
The output voltage is…
Part Number: TPS51916 How to contorl TPS51916's power-up ,because we use it power our cpu at the same time, but our cpu has a power-up sequence.
thanks very much!
Part Number: TPS51916
Hi team
My customer want to change the IC from RT8231AGQW to TPS51916RUKR .
I want to change the IC that is applied to Intel CPU EVM.
Is there a problem when I change it?
Thank you.
Part Number: TPS51916
Hello TI Experts,
1. Please tell me why is the ability to change the switching frequency of the TPS51916? When can I need her? And how to determine which switching frequency is necessary for my processor and RAM?
2. Which version…
Part Number: TPS51916 Other Parts Discussed in Thread: TPS3808
Hi ,
We are facing an issue with the components having Thermal PADs. The issue is that the excess solder paste on the thermal PADs causing malfunction to the part which eventually resulting…