Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS51916
Webench support team,
I can't get a simulation result due to the specification limitation of the external FET used in Webench-Power-Designer. The below is an error message…
Part Number: TPS65273V Other Parts Discussed in Thread: TPS51916 Hi Experts,
I have project using TPS65273V driving Xilinx UltraScale FPGA to provide voltage for DDR3 control
I have calculated the component value according to Datasheet and I want to ask…
Other Parts Discussed in Thread: TPS51916 HI,
I just hooked up my TPS51916EVM in the lab for the first time. I have no output on VDDQ, VTT or VTTREF. I am seeing 1.5A on the V5IN input with S3 and S5 turned off. The device got extremely hot so I shut it…
Part Number: TPS53015 Other Parts Discussed in Thread: , TPS51215A , TPS51916 Hi, support team
My customer has the questions as follow:
There's an D1 BAT54XV2T1 in TPS53015EVM-126. According to the follow post, I know that it clamps the negative voltage…
Part Number: CSD86360Q5D Other Parts Discussed in Thread: TPS53015 , TPS51916 , TPS51215A , CSD87335Q3D , CSD87384M , CSD87588N , CSD87352Q5D Hi sir,
Can I use FET (CSD86360Q5D), in the following design,
is there any issue?
Design[1]
Use IC: tps53015
VIN…
Other Parts Discussed in Thread: CSD86330Q3D , CSD87330Q3D I am trying to save some cost and PCB area by going to an integrated power stage and was wondering if the CSD86330Q3D power block can be used in place of the discrete high and low side FETs in my…
Other Parts Discussed in Thread: TPS51916 , CSD87331Q3D , PMP5922 Hi,
I need a reference design for DDR3L power solution using the following components:
TPS51916
FET driver csd87331q3d
Inductor XAL6030-102MEC 1uH
Vin= 5v
Vout=1.35v @ 5A max
Iout limit…
Other Parts Discussed in Thread: TPS51916 , TPS51216 Hello,
I want to do a design for DDR3 using the TPS51916.
The data sheet specifies "Conversion Voltage Range: 3 V to 28 V", I am not sure if this means for all output voltages (VDDQ, VTT, VTTREF) or…
Other Parts Discussed in Thread: TPS51916 , CSD86330Q3D I'm designing power part, TPS51916 is best part for me.
Could I get reference design of TPS51916 for DDR3 with VIN=5V as following conditions?
(1) D-CAP2, 670KHz, Tracking Discharge mode
(2)…
Other Parts Discussed in Thread: TPS51916 We are looking to use the TPS51916 in a 3.3V-1.5V (plus VTT) DDR3 application. It will be supporting 2 banks of 72 bit DDR3 (9 devices).
First: It appears the V5VIN current is always <1mA regardless of load or…