Part Number: TPS53015TPS53015DGS
Our company uses four TI TPS53015DGS as 4.2V,3.8V,5V and 3.3V. The working voltage range required in the specification of this power supply is 4.5-28V. The test found two serious problems, so it cannot be used normally…
Part Number: TPS53015 Other Parts Discussed in Thread: CSD17507Q5A , CSD86336Q3D , CSD86350Q5D , CSD87351Q5D Hi,
We are planning to use TPS53015 part in our board. Our system requirements are listed below.
1. 19V input (+/-5%), 3.3V Output Output Current…
Part Number: TPS53015 Other Parts Discussed in Thread: TPS53014 Hi
I'm designing a power circuit using TPS53015.
I'd like to check the operation of the circuit using TINA simulation, but there is not TINA model for TPS53015 on the Web site.
…
Part Number: TPS53015 My customer is trying to reduce component count on TPS53015 design. Are both the zener + Rclamp and snubber circuit necessary on the switch node? Or is one sufficient for reducing SW node ringing - which is recommended? Our application…
Part Number: TPS53015 Hi Team,
Below is my schematic, I find the Vout noise when switch is doing switching. Could you let me know the method could eliminate noise?
yellow : Vout (CO1)
red : switching node
Regards,
Roy
Part Number: TPS53015 Other Parts Discussed in Thread: LM27403
Hi,
The input voltage is 12V, and the output voltage is 5V, please teach me the appropriate value of the input/output capacitor. The inductor is 10uH. When the output voltage of EVM is 1.05V…