Part Number: TPS53015 Hi Team,
One of my customers is currently facing issues with our TPS53015. They are experiencing lock out when they try to power on after an immediate power outage. These are their specs:
Vin = 24V Nominal, 15V at Sleep mode, can…
Part Number: TPS53015 Other Parts Discussed in Thread: TPS53014 I am attempting to measure a bode plot on a DCAP-2 device, TPS53015, for stability testing.
I came across the following e2e post, which describes a method for bode plot measurement requiring…
Part Number: TPS53015 Hi team,
My customer wants to use the device tps53015 to change 12v to 1V 15A. But the datasheet doesn't give the gate driver sink and source current spec. Could you please give the suggestions and reasons?
Thanks.
Hello Zelimir,
Just to make sure I understand your request, the TPS53015 is not a supply, it is a synchronous buck controller.
Can you please provide the care abouts?
Thanks!
Tahar
Other Parts Discussed in Thread: TPS53015 Hi
In electrical characteristics of TPS53015's datasheet,
there is description about Vreg5 like attached document.
I think this is electrical characteristics when Ta is 25℃.
But if Ta changes, does they change…
Other Parts Discussed in Thread: TPS53015 Hi everyone,
I have built a buck converter using TPS53015. Input voltage is 24 Vdc, output voltage is set to 5 Vdc and desired maximum output current is 15 A. However, the efficiency of the built system is approximately…
Part Number: CSD86360Q5D Other Parts Discussed in Thread: TPS53015 , TPS51916 , TPS51215A , CSD87335Q3D , CSD87384M , CSD87588N , CSD87352Q5D Hi sir,
Can I use FET (CSD86360Q5D), in the following design,
is there any issue?
Design[1]
Use IC: tps53015
VIN…
Other Parts Discussed in Thread: TPS53015 , TPS54429 , TPS54525 , TPS53125 Hello,
My coustomer searching solution to implement 'remote sense' at the devices TPS53015,TPS54429,TPS54525.
If they can use remote sense function, let me know how to use.
…
Hi Aki,
You can get lots of single channel results on ti.com, product searching... Like TPS40195, TPS53119, TPS40075, TPS53015...
Yes, for TPS51225, the output voltages are fixed.
Regards,
Hao