Part Number: TPS53625 Hello,
Customer test intel spreadsheet. When output voltage decay to 0.64V on 10A, The alert not assert. Per spreadsheet, it needs to decay about 0.59 V the will send alert. But the output of TPS53625 can't decay more below…
Part Number: TPS53625 Hello,
We found the VCCPVNN transient out of intel spreadsheet spec on light & heavy load. And when we check phase node we found there has double pulse behavior.
We have change PR133 from 6.34k to 30 ohm for zero load…
Hi Dylan,
TPS53627 controller support only 10mV step, not support for 5mV step. If intel CPU support only 5mV step, it is suggested to use TPS53626 controller.
The main difference between TPS53625 and 626 is, TPS53625 support only VR12.0, not VR13. TPS53626…
Part Number: TPS53622 Other Parts Discussed in Thread: TPS53625 , Hi all, My customer needs to build a power stage system for an Atom Intel C3000. At first the system was made up by: TPS53625 + CSD97370; with a 18V supply. --> unsatisfactory results. The new…
Hi Chasel,
Thanks for the response.
Please confirm, We have Harcuvar CRB which has TI VR12 controller i.e TPS53625
Now I can re-use the platform and BIOS and core boot provided by inetl for Harcuvar CRB
and there will not be any firmware or SW impact…
Part Number: CSD95379Q3M Other Parts Discussed in Thread: TPS53625 , TPS53647 , TPS53622A Hi
I just started design of TPS53625 power supply and came to notice that it needed output power stage MOSFET, why is this needed.
My requirement is Vout: 2.3V and…
Patrick,
TPS53625 is a proprietary solution. Can I ask you to contact imvp@list.ti.com directly? Please reply here so I can remove your post from e2e.
Thanks,