Part Number: TPS54160A How is relationship between VIN and VOU
for example, i want to design a circuit that OUTPUT is 6V .
The VIN minimum is 6+(voltage reference 0.8)=6.8V right?
Part Number: TPS54160A Customer is referring to SLVA369A for the split-rail power for 24Vin to +/-15Vout/0.3A.
Could you help to review the schematic below? I think it would need one more 10uF capacitor connected between VIN to PGND on schematic since…
Part Number: TPS54160A Hi,
C80: Ceramic capacitor (_3225, 80V, 4.7uF, ±10%) and C6: Ceramic capacitor (_1608, 50V, 1uF, ±10%) We are investigating whether it is possible to remove two parts.
Before and after removing the parts, the following checks…
Part Number: TPS54160A Other Parts Discussed in Thread: TLV841 Hello,
I am an FAE for a distributor that handles TI products. I received the following question from a customer about the TPS54160A. (Question) I want the EN pin to ramp up slowly. Is it…
Hi Daniel
Thanks for the reply
I got what you have done but why are we calculating gain at 10hz is there any specific reason?
Also by taking 4.7nf and 100Mohms i got pole at 0.334hz and at 10hz i am getting -29.52dB which doesn't match your answer…
Hi Vishwanath Tigadi,
Thanks for your replay.
I have noticed that at the output we have 2 capacitor and have changed it to 1 capacitor of value 47uF and 10mohms by adding custom component.
The result i have return above have the circuit given below…
Part Number: TPS54160A Please elaborate on the following discrepancy:
1-1) In SLVA369A–October 2009–Revised October 2012 Eq 13 and 15 use (2*Fsw*Lo) as a denominator. In the excel file, however, formulas in C73, C75 lack the multiplication by 2 (ex…
RC snubber is often utlilized for noise reduction in sw waveform. Parastic LC tank in IC has resonanat frequency which results in ring on sw waveform. RC snubber is utilized.
From my experience, isnt strict methodical approach for tuning LC for buck…