Part Number: TPS5420 Other Parts Discussed in Thread: , TPS54240 I am currently using the TPS5420 in and automotive app to regulate battery voltage (9-15volts) to 5 volt. I need ~1A capacity.
I need lower quiescent current so looking at TPS54240 or TPS54202…
Other Parts Discussed in Thread: TPS5420 , LMZ21700 , TPS54202 , LMZM23601 , LMZ21701 , LMZM23600 Thanks for the info.
Two other ?'s
I have used the TPS5420 in a application for years with no issues. In a revision, I tried using a LMZ21700 module. …
Part Number: TPS5420-EP
Hello ,
We have a need on the TPS5420-EP (10.000 PCEs / Year), but before we need more technical informations about the BiCMOS LBC4 BOA process technology :
-The feature size : 0.35 µm , 0.32 µm ??
-The substrate…
Part Number: TPS5420 Other Parts Discussed in Thread: LM5117 , TPS54240 Is it possible to get stable operation of the TPS5420 buck converter by measuring the output current via a sense resistor and MAX4372H current sense amplifier (for example), and feeding…
Part Number: TPS5420 Dear TI Team,
One of my customer have the issue below:
The point being tested is U22 foot number 8. It can be seen that the pk-pk voltage is unstable and there is a random drop to 26 V
causing a signal drop below 100,000 and high…
Part Number: TPS5420 Other Parts Discussed in Thread: TPS5430 , TPS5410 Hi.
There is no the ESD Rating in TPS5420's datasheet.
But, TPS5410, TPS5430 has the ESD Rating.
Why no ESD Rating in TPS5420's datasheet and what is TPS5420's ESD Spec?…
Part Number: TPS5420 Hey Everybody,
what would be the reasons if I just get 0.8 volt at the output of my EVM tps5420evm-605 !?
Input 12vdc lab power supply with 3 amp current cut\load =15 ohm 20w\ expect to see 3.3 volt by having R_Vsens=R6=31.6k but…
Part Number: TPS5420 HI
The circuit is composed as follows using the TPS5420. VIN: 24V -> VOUT 5.2V, IOUT 1.5A This IC operates OCP operation in HICCUP MODE. TI recommends that ICs that operate OCP operation by LATCH-UP be used.
Part Number: TPS5410 Other Parts Discussed in Thread: TPS5420 , Please can you let us know the manufacturing process (e.g. CMOS) and silicon geometry for TPS5410 and TPS5420.
Thanks.
Dave