Part Number: TPS54228 Hi team,
Could you give me comment on following customer question? I assume the datasheet describes the thermal pad of the DDA package (HSOP) must be connected to GND, so the answer is no. If it's possible, could you give me advice…
Part Number: TPS54228 Tool/software: WEBENCH® Design Tools In following condition
Vin=6.2V, Vo=5.0V, Io=1.5A
Design can not be create by webench.Please let us know the reason.
Part Number: TPS54228 Hi,
In TI datasheet talked about SGND and PGND but in them layout it’s seems that it’s not implemented:
in my layout i think that need to separate the SGND and PGND like the red line, please advise:
Part Number: TPS54228 Other Parts Discussed in Thread: TPS54428
Hi support team,
I have a question about TPS54228. The output voltage of TPS54228 can be set by R1 and R2 according to equation (3) in the datasheet. What is the behavior of the output voltage…
Part Number: TPS54228 Hi Everyone!
I have two questions about datasheet Package Dimensions:
Q1)What kind of measurement is used for the measurement that guarantees the standoff amount of 0.00 mm to 0.15 mm?
Q2)Is the sample at the time of measurement a…
Part Number: TPS54228 Hi
because the MOSFET are in the converter, the spec only show the SW(low side MOSFET) max voltage=22V.
We want to know the high side MOSFET max voltage=?
Thank you!
Other Parts Discussed in Thread: TPS54228 , TPS54325 We have questions about TPS54228.
Question 1.
Can TPS54228 meet following conditions?
Condition 1.
Vin=12V
Vout=1.0V
Iout=1.2A
Output voltage accuracy + ripple voltage + load transient = within ±3%…
Part Number: TPS54228 Other Parts Discussed in Thread: TPS561201 , INA199 , LM321 , LMV431
Hello,
I would like to add another circuit as the attached rough schematic in order to limit the current of tps54228 to 1A. I assumed that it will influence sw pin…
Part Number: TPS561201 Other Parts Discussed in Thread: TPS54228 Hi, Team.
i've been asked by Customer , please support it.
1. Why doesnt TPS561201 need to have capacitor even TPS54228's VREG pin needs?
Cap on VIN(TPS561201) works "cap for VREG…