Part Number: TPS5430 Tool/software: Dear Sir / Madam,
PN: TPS5430DDAR
We observed the thermal pad has discoloration/oxidation. Could you help to check if this kind of issue is normal for these parts?
If you have a PCN document for explanation on…
Part Number: TPS5430 Tool/software: Hello,
I am using the TPS5430 in my design, and I need to understand the response time of the overvoltage protection.
Could you please provide details on how fast the TPS5430 turns off the output when OVP is triggered…
Part Number: TPS5430 Other Parts Discussed in Thread: LM2596 Tool/software: Greetings,
I am using TPS5430 for converting 15 VDc to 5 VDc. The circuit is working fine but is there any short circuit protection method to prevent thermal overrun or prevent…
Part Number: TPS5430
Tool/software:
Dear TI experts and gurus,
Could you help me review this circuit, which i designed and followed the methodology in "sszt824" doc of "Design a Second-stage Filter for Sensitive Applications"? For my senario which…
Part Number: TPS5430 Tool/software: Hi Sir,
Using TPS5430 can we achieve the following power stability
Power Stability : Unit- % ( RMS ,8 hrs, Range : 0.02 - 0.25)
Unit- % ( Peak to Peak ,8 hrs, Range : 0.1 - 1)
Part Number: TPS5430 Tool/software: Im trying to simulate the bode plot for TPS5430 with ceramic output capacitor. When I update the ESR of output capacitor as 0 ohm in Webench power designer, the phase margin fails. I saw the application note of slva237c…
Part Number: TPS5430 Tool/software: Hello,
I am working on to design power supply output 5VDC with the help of TPS5430DDA converter. Input voltage = 12VDC, Iout = 1.63A.
It was already in use in our design below the circuit.
The new design requires…
Part Number: TPS5430 Tool/software: Hi TIer
Customer use our TPS5430DDAR like this schematic.
Output is 9V (250mA - 450mA)
The customer will get some abnormal SW waveform similar to DCM mode in a normal SW waveform with a switching frequency…