Other Parts Discussed in Thread: TPS54318 , TPS54319 Hi,
Please let me ask about Enable threshold of TPS54319. I understand that there is no min/max value in electrical characteristics and so it can't guaranteed. But I know TPS54318 is similar device of…
Hi Elleen, Thanks for your response, Kindly confirm that the APP Note Calculator can support TPS54623RHLR. Over in the Excel sheet it was mentioned that this file supports the Below mentioned parts only.
TPS54218
TPS54318
TPS54319
TPS54320
T…
Other Parts Discussed in Thread: TPS54319 , TPS54318 Hi,
We are planning to use TPS54319 part in our new design. We are looking for webench support for this but it is not available. Why this part is not supported in Webench?
But we have seen TPS54318 support…
I'm not sure I would recommend that for TPS54319. You are free to try it though. I would expect erratic start up, with current limit active. I may give it a try tommorow or Monday.
Part Number: ADS42JB69EVM Other Parts Discussed in Thread: TPS54319 , LMK04828 Hi everyone,
The 'Power Supply' page in ADS42JB69EVM design shows that it converts '5VIN' DC voltage to '4V' with 'TPS54319' module, and then change '4V' to …
Other Parts Discussed in Thread: TPS54319 What would you suggest to eliminate these voltage spikes on the input side of the TPS54319EVM?
Setup
Hardware: TPS54319EVM
Vin: 3.3 V Vout: 1.8 V Iout: 1 A (resistive load)
Results
Vin
Vin (zoomed)
.
Other Parts Discussed in Thread: TPS54319 , TLV62085 , TPS563200 Hi Sir,
My customer usually ask me one question, but i still can't clear answer him.
Question is if we use buck converter application input 5V, output 3.3V / 3A, usually we select TLV62085…
That part is supported out of or MCP team in China. If you email me at j(dash)tucker(at)ti(dot)com I can forward your request to my contacts on that team.
The solder requirements are somewhat generic. They are from our packaging group and are tied…
Other Parts Discussed in Thread: TINA-TI Update of TINA9-TI Spice Model Libraries and Example Circuits
This note describes the step-by-step process for updating the TINA9-TI Spice Macro Libraries and Example circuits. The update is initiated by selecting…