Part Number: TPS54340B-Q1 Tool/software: On simulating Dc- Dc Converter section, I find the error as stated below on importing spice model of TPS54340B-Q1 module from website.
Could you please share the encrypted version of TPS54340B-Q1 modul e So that…
Part Number: TPS54340B-Q1 Tool/software: Hello,
I am using TPS54340B-Q1 in my design. we are converting 24v to 3.8v using this IC. during radiation emission test we observed that we are getting more radiation from this IC. can you please support me…
Part Number: TPS54340B-Q1
Tool/software:
Hi E2E,
In order to reduce the current of the entire product.
we modified the pull-up resistance and pull-down resistance of EN and FB.
R8=324K;R9=NC;R12=62K; R10=560K;R13=220K
Is this parameter reasonable…
Part Number: TPS54340B-Q1 Hello,
I am using TPS54340B-Q1 to convert 24V DC to 5V DC the load current is 3A.
For 5V output i am getting 9.3V at the output.
Please help me to rectify the issue, Refer to the below schematic.
Part Number: TPS54340B-Q1 Other Parts Discussed in Thread: TPS54340-Q1 Hi TI support,
We are using TPS54340B-Q1 in one of application with design details of VIN=12V to 18V & Iout max=2.5A, Vout=4V, Fsw=917KHz. Input voltage is fixed at 15V. There…
Part Number: TPS54340B-Q1 Other Parts Discussed in Thread: TPS54340B , Hi Team,
Is there any deference point between TPS54340B and TPS54340B-Q1? Can I evaluate TPS54340B instead of TPS54340B-Q1?
Regards,
Kotaro Yamashita
Part Number: TPS54340B-Q1 Other Parts Discussed in Thread: TPS54360-Q1 , TPS54340-Q1 , , TPS54360B-Q1 Dears:
Our customer uses TPS54340-Q1 and TPS54360-Q1, and these PNs are NRND.
I promote TPS54340B-Q1 and TPS54360B-Q1, there is an issue about the…
Part Number: TPS54340B-Q1 Hi TI support,
Due to EMI concerns we are trying to add Rsnub=3.0E & Csnub=1100pF in TPS54340B-Q1 based design as shown in attached schematic. Place of their addition is highlighted with red line. Design details are VIN=10…
Part Number: TPS54340B-Q1 Tool/software: WEBENCH® Design Tools Hi TI support,
I recently made the design using TPS54340B-Q1 with details as under,
VIN=12-18V, Vout=4.0V, IOUT=2.5A max, Tamb=60'C, Freq=918KHz. I replaced the compensation components…
Part Number: TPS54340B-Q1 Hello TIer,
Could you help us to provide TPS54340B-Q1 minimum off time? Looks webside show Dmax is 98% at what switching frequency condition?
In our design output voltage design 8VDC and Input range from 9VDC to 16VDC.