Part Number: TPS54362-Q1 I'm trying to design a simple 3v3 2A supply using the subject part number. There are so many errors on the data sheet that I do not have confidence in it. Is there an updated datasheet, or can someone share the 3.3v passives values…
Part Number: TPS54362-Q1
Hello,
Attached output ripple waveform in datasheet.
There are only output current 0A, 100mA, 1A and 3A.
Could you provide this ripple waveform at Io=200mA, 300mA, 400mA,....900mA?
Or could you let me know at which…
Part Number: TPS54362-Q1
I've got a similar problem with ripples ON OUTPUT OF TPS54362, my question is if the frequency FSW adjusted to be 555KHz, why the ripples frequency is 1.125MHz, REPEATED by 735Hz
how can I check my adjusted frequency? and…
Hello Eli, sorry for the delay. The errata as written was for Revision A. Revision B has been tested under the same conditions without issues, however the points in the errata are still recommended as a best design practice even for Revision B. Please…
Part Number: TPS54336A Other Parts Discussed in Thread: TPS54360 , TPS54362-Q1 Hi Team,
Can use the negative voltage circuit diagram of TPS54360 for wiring to TPS54336A do negative voltage? VIN: 20~24V Vout: -15V/0.6A
Hi
I have TPS54362 Q1 with VOUT = 5V and 10V. They running in DCM mode but only when VIN is less than 28V, after that it the current jumped more than 10mA (without load).
I checked the datasheet and there nothing mention or explained coming out from…
Part Number: TPS54362-HT Other Parts Discussed in Thread: TPS54362BEVM , Hello.
I am interested in TPS54362-HT, but I want to test before including it in my schematic. This part number has no development kit but I found the TPS54362BEVM development…
Other Parts Discussed in Thread: TPS65320-Q1 , TPS54362-Q1 I would like to confirm the function of VIN_LDO of TPS65320-Q1.
In the datasheet, when LDO and Buck converter is enabled, LDO input is switched the buck converter output.
In the case of LDO…