Part Number: TPS543620EVM Other Parts Discussed in Thread: TPS543620 Hi Team,
I am Jayden, I have some question about overcurrent protection when I run TPS543620EVM in the lab.
1. Why the fsw in high current limit is lower than in low current limit wh…
Part Number: TPS543620EVM Hi team,
I'm Jayden, I have some questions about enable and adjustable UVLO when I run the EVM in the lab.
The waveform on the left shows EN is float without RENT and RENB. Only the pullup current Ip sets the default state…
Part Number: TPS54J061 Other Parts Discussed in Thread: TPS543620EVM , TPS543620 For the TPS54J061 to generate from 12Vin the following voltages:
0.95V or 1.03V (~2A or more) +/-30mV tolerance
1.8V (~3.5A or more) +/- 90mV tolerance
Others such as 1.2V…