Part Number: TPS54386
Dear TI
I read TPS54386/TPS54386-Q1 Datasheet and find a mistake in datasheet!
MSS1278-153ML is 15uH. but Datasheet talk to use 22uH!
Which is it right? 22uH?
Best regards.
Part Number: TPS54386-Q1
Hi
We have a design for automotive. When we test EMI performace, it failed. Below picture are the testing result and schematic. Can you give some advise ?
Anohter, if L30 & L31 instal ferrite bead, the system can't operate. But…
Part Number: TPS54386 Tool/software: WEBENCH® Design Tools Hi,
Why can't find the WEBENH entrance of this device? is there other way to simulate this device?
Part Number: TPS54386
Hi team,
My customer is looking for a +10V 3A & -8V 3A dual channel power supply for OLED screen. I'm wondering is it possible to make it happen with dual channel buck like TPS54386. I've do tests on TPS54386 EVM and…
Part Number: TPS54386-Q1 Hi e2e,
Good day.
We have a customer asking for the “Absolute Maximum junction Temperature” for TPS54386TPWPRQ1?
Is it the same as the max “Operating Junction Temperature”of 125C?
Also, he is looking for…
Part Number: TPS54386 Dear Texas team,
This is the continuation from this post: https://e2e.ti.com/support/power_management/non-isolated_dcdc/f/196/p/645543/2381672#2381672 which is locked but not solved yet. Unfortunately Argentina official agent in charge…
Sunil,
That is just the schematic from the users guide. I would expect you had to make your own schematic and PCB layout using your own CAD system correct? What are you using for printed circuit boards?
Part Number: TPS54386-Q1
Dear,
our client power spec as below:
Vin:12V
output1: 1.2V/2A output2: 3.3V/2A
AECQ-100
we will propose TPS54386-Q1, have any concern in design spec to note?
IF any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence…
Part Number: TPS54386 Dear TI,
My name is Bruno and I'm from Argentina.
I have designed a product which use TPS54386PWPR to provide 5v and 6v. The first one is for digital modules and the second one for a small air compresor controller. The thing is…