Part Number: TPS54394 Hi expert,
My customer found the issue about softstart waveform, which has unsmooth ramp up scenario.
I also find the scenario in TPS54394 datasheet Fig. 11 as bleow red square frame:
My custmoer meet the issue in -25℃, 25 ℃, but…
Part Number: TPS54394 Other Parts Discussed in Thread: TPS542941 , Hi team,
what's the difference between TPS54394 and TPS542941 aside from the current rating and Rdson,
are they BOM to BOM if the loading is below 2A,
anything I miss?
Part Number: TPS54394 It's funny on one thread regarding this part, someone said the user's layout was very bad because the switch node was connected to the inductor using a different layer. That is the (poorly) recommended layout on page 16 of the data…
Part Number: TPS54394 Hi,
Please could you give me some feedback on the following design.
TPS54394
1V1 @ 3A
1V5 @ 3A
Most parts have their ratings on the schematic.
L1 & L2 = ABRACON ASPI-6045T-2R2N-T
Here's the layout:
There are internal layers…
Part Number: TPS54394 Other Parts Discussed in Thread: TPS62130 , TPS62903 Hi,
Looking at page 14 of the datasheet the peak inductor current is calculated at 3.46A.
Trying to replicate the design in webench, I get a value L Ipp of 2.08A.
Can you advise…
Part Number: TPS54394 Other Parts Discussed in Thread: TPS54494 , TPS54294 , TPS542941 Are there any parts like TPS54394RSAR, QFN footprint and pin out but that run at a higher switching frequency?
In the 2A to 4A output range, it doesn't exactly need to…
Part Number: TPS54394
Hello E2E,
Please help to review the design below and kindly share your feedback. Our customer tried implementing the circuit in real life to see if it works, but they don't have the appropriate tools to solder everything at the…
Part Number: TPS54394 Hello Ti,
I am using TPS54394 for 1.8V output, and we found the output vlotage is abnormal and powergood drop.
Please help to clearify.
Thanks!
David