Part Number: TPS54519 Other Parts Discussed in Thread: TPS54218 , TPS62867 Hi,
For TPS54519, Any recommendations for soft-start time range ?
In TPS54218 datasheet, i can see below recommendation for SS time.
Thanks and Regards,
Pedaiah G.
Part Number: TPS54519 Hi Team,
Good day.
A customer is using trying to simulate TPS54519 Buck converter in tina TI with input voltage of 5v and required output voltage ov 1.8v however, they are not able to get 1.8V output voltage.
The models used are from…
Part Number: TPS54519 Other Parts Discussed in Thread: TPS54678 , TPS62867 The VSENSE pin is used to sense the output voltage through a resistor divider set to 0.6V (typ) The pin's actual sense limits though are 0.594V(min) 0.600V(typ) 0.606V(max) from…
Part Number: TPS54519 Hi,
TPS54519RTER Part i am using for dynamic power which is switch between 0.9V and 1V. so i want to know based on what the intended crossover frequency will be decide.
In datasheet take 70KHz based on what ?
I am new to close loop…
Part Number: TPS54519 Other Parts Discussed in Thread: TPS62088 , , TPS62816-Q1 Hello Expert,
I have already used that Design Tool for Output Voltage Adjustment Using a DAC for TPS62088.
Can I use TPS54519 like TPS62088 as below?
If yes, could you give…
Part Number: TPS54519 Hi,
We have run into an issue where a non-TI produced component is out-of-stock and the PCB has been already designed. I am looking for pin-to-pin compatible alternative component and the TPS54519 seems like a good one, however,…
Part Number: TPS54519 Other Parts Discussed in Thread: TPS568230EVM , TPS62867 , TPS568230 Hello,
I have a question on TPS54519 layout. From my previous experience, AGND of IC should be connected on single point with GND (PGND) to prevent switching noise…
Part Number: TPS54519 Other Parts Discussed in Thread: TINA-TI , TPS62869 Hello,
I am currently trying to design a step-down dc-dc converter with TPS54519.
The fact is that after reviewing the datasheet I am not able to design the compensation network…