Part Number: TPS54560-Q1 Other Parts Discussed in Thread: MIDAS Tool/software: Hi
We have the following issue with the controller of our speed pedelec, after it being used for over a year without any issues, we now start seeing with some bikes that while…
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: LM76005 , Dear team,
I am searching for p2p alternatives to TPS54560QDDARQ1: can you please share orderables that can fit as a drop-in replacement?
AEC-Q100 is not mandatory
Best regards, Antoin…
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560B , , LM61495-Q1 , LM61440-Q1 , LM61460-Q1 , LM61440 , LM61460 , TPS54560 , TPS54560B-Q1 Dear Support Team,
my company has succesfully used the TPS54560B IC in the design attached for a 12V to 5V…
Part Number: TPS54560-Q1
Hello,
I built a test board for TPS54560-Q1 base on schematic below. and when I power it on, the output voltage is < 1V.
I want to konw what is the reason it behaves this way. I checked every connections, the voltage on pin…
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560 Hi
Standby power consumption is now tested at 10mA. Is there any good suggestion to reduce power consumption?Thanks!
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560B-Q1 , We are using the TPS54560-Q1 down-converter in our design pretty successfully, however a new set of boards arrived and about a 1/3rd of them the device blew up when applying power …
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: LM25117-Q1 , LM5146-Q1 I'm using the TPS54560-Q1 Step Down DC-DC Converter the input is 24V the output is 5A/5V, do I need a fan or/and thermal pad to help cooling the device.
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560 , TPS54560B
My customer use TPS54560-Q1 in their power board. About one-sixth of the defective rate of trial-produced products. The Vin is 12V and the designed output is 5V, but the output…
Part Number: TPS43061 Tool/software: WEBENCH® Design Tools Error message if we change the input range but beyond the limits, example shown below.
"Design cannot be created! Your preferred device does not work with the inputs you selected." …
Hi RA,
Thank you for the update.
For the TPS54560-Q1 device product folder( https://www.ti.com/product/TPS54560-Q1 ), you will see the notation below.
Looking at your max input voltage range, it looks like you would want a 60V device.
I would suggest looking…