Part Number: TPS54560B-Q1 Tool/software: Dear TI-support team,
is it possible to connect two or more TPS54560B-Q1 ICs in parallel in order to get more output current?
The output is current-mode controlled and the COMP pin is available so two COMP pins…
Part Number: TPS54560B-Q1 Hello,
I am using the two Buck -TI part TPS54560BQDDARQ1 for the DC-DC converter. One for the output 12VDC /5A and second is for 5VDC/5A.
My input is 9V-32VDC.
I have attached my schematic is below. when I am checking the output…
Part Number: TPS54560B-Q1 Other Parts Discussed in Thread: TPS62933 We made our custom power distribution board for a micro drone.
The board is supposed to supply:
20A at 17.4V to a 4in1 ESC (powering 4 BLDC motors) max - Battery
5V to flight controller…
Part Number: TPS54560B-Q1 Other Parts Discussed in Thread: TPS54560B Hi Sir,
if any reference design based on this IC(TPS54560B) which can pass E Mark? or have other suggest part number that pass e-mark certification, thnaks.
Part Number: TPS54560B-Q1 Other Parts Discussed in Thread: TPS54560-Q1 Hi,
On the website, TPS54560B-Q1:is automotive part. but there is no "AECQ100" in the datasheet.
Is TPS54560B-Q1 AECQ100 part?
Thanks and best regards,
Part Number: TPS54560B-Q1 Hi,
l have designed a buck converter using TPS54560BQ with following specifications:
VIN : 48V
Vout: 24V @ 5 Amps
Continuous current at 24V : 2.5 Amps
Ambient temperature: 45 deg Celsius
Schematic is copied from Power designer…
Part Number: TPS54560B-Q1
Based on the PPAP document for the Part number TPS54560BQDDAQ1 it appears that tests have been conducted for EM, TDDB, HCI and NBTI to the JEDEC standards.
Do you perform the below tests for each part, or per family, or per…
Part Number: TPS54560B-Q1 Hello TI, I have designed a circuit using TPS54560BQDDARQ1, DC-DC converter. Operating input voltage is 24V (From manual SMPS). We designed circuit to get output voltage is 3.3V . The circuit is same which was given…
Part Number: TPS54560B-Q1 Hello
Are the following devices Isolated or Non isolated:
TPS54560BQDDAQ1 and TPS54560QDDARQ1
What does the B stand for?
Best Regards
Nigel