Part Number: TPS54628 Hi
because the MOSFET are in the converter, the spec only show the SW(low side MOSFET) max voltage=22V.
We want to know the high side MOSFET max voltage=?
Thank you!
Part Number: TPS56428 Other Parts Discussed in Thread: TPS54628 Dear Experts,
Condition: Input 12V, output 3.7V, loading 2.5A
We found high side Vds of TPS54628 will be about 18V.
Is TPS54628 high/low Vds rating the same as 20V (22V<10ns)? Could you help…
Other Parts Discussed in Thread: TPS54628 , TPS54328 We have a question about TPS54628.
Please show us the data of package size of TPS54628.
We can't find the information of package size and figures in the datasheet.
Best regards,
Takahiro Nishiz…
Other Parts Discussed in Thread: TPS54628 , TPS54328 We have a question about TPS54628.
In datasheet p.13 Table 1,
68µF is recommended about output capacitor.
And we want to use the aluminum electrolytic capacitor to suppress load transient.
Can…
Hello Tateo,
Regarding how to decide how to configure the rise time. It is very application dependent. That said there are key parameters that you want to pay attention to.
-Know the cumulative capacitance on the output net of the TPS54628 and design…
Part Number: TPS54628 Hi,
We got a question from customer about TPS54628. Could you help us?
[Question] How much is the delay time between detecting current limit and turning off the FET? They don't need gurantee. They will use it as reference.
Best…
Part Number: TPS54628 Hi,
We got a question from customer about TPS54628. Could you help us?
[Question] When the device is start-up under output short to GND, what is the behavior of IC? During the device is in soft-start period, does the UVP protection…
Part Number: TPS56C215 Other Parts Discussed in Thread: TPS54628 , TPS56C231 Dear team,
Customer use TPS56C215 and design enable signal voltage level at 1.23V. Now faced to some issue if our device threshold voltage is 1.3V which is to equal datasheet…
Part Number: TPS56428 Other Parts Discussed in Thread: TPS54628 Hi,
I want someone to review the layout of TPS54628. I can share files offline.
Thanks
Tanveer