Part Number: TPS548A28EVM Other Parts Discussed in Thread: TPS548A28 Hi Team,
This EVM work properly at the ambient temp of 80℃? What temp this EVM can tolerant by?
Thanks,
Shoo
Part Number: TPS548A28EVM Other Parts Discussed in Thread: TPS548A28 Hi Team,
While customer is evaluating TPS548A28EVM, anunexpected operation is observed.
At 4VIN, TPS548A28 cannot drive 13~15A load. Vout is reduced and repeats ON and OFF. It doesn…
Part Number: TPS548A28EVM Hi Team,
We are using TPS548A28EVM and set to 800kHz FCCM mode, Vin=12V and no load here. We measure the switching frequency will be around 950kHz. However the datasheet introduce the switching frequency range will be 720kHz…
Part Number: TPS548A28EVM Hi TI team
I buied a TPS548A28EVM and tested the transients load response, The testing reslut are different with those in the 2.6 chapter of the user's guide .
My testing load is same with the guide, 2A/us, 4A to 11A.Please see…
Hi Humberto,
When you used the TPS548A28EVM under your load setup the device was able to deliver the load right? And when you switched to the TPS54J061 there was no issues there? Best, Ryan
Part Number: TPSM8A28 Other Parts Discussed in Thread: TPS548A28 , TPS548A28EVM Hi Team,
My customer wants to use TPSM8A28 in their system as 3.3V power input condition. Do you think there are any risks such the use case? I can not check it on Webench since…
Part Number: TPS548A28 How stable is the output voltage of the TPS548A28 when the input voltage is 3.3V and the output voltage is between 0.6V and 2.5V?
The stability of the output voltage of the TPS548A28 is relatively constant between 0.6V and 2.5V…