Part Number: TPS54A20 Hi expert,
when operating in 2-phase interleaving mode, I'm interested in what would happen during load transient.
For example, when very large and high slew-rate load step-up comes, the control loop easily goes into saturation…
Part Number: TPS54A20 Other Parts Discussed in Thread: UCD90160A Hi ,
In my design the ennable pin of TPS54A20 is driven from a GPIO of another power device as below:
TPS54A20 ennable is driven from a device that can start after the 12V power supply…
Part Number: TPS54A20
Hello team,
My customer has some questions about the pin connection of the TPS54A20.
Does 11pin (NC) need to be connected to 20pin (SCAP)? The data sheet describes as follows in the pin functions.
“NC: No connect. This pin is…
Part Number: TPS54A20 Other Parts Discussed in Thread: TINA-TI Team,
Customer has a stability problem with TPS54A20 and want to ana;yze the design to get the theorethical phase margin and gain.
-The older webench (flash based) enables to simulates this…
Part Number: TPS54A20 Other Parts Discussed in Thread: TINA-TI Tool/software: WEBENCH® Design Tools To whom it may concern,
I need to evaluate adding a ferrite bead in series on the power path.
I have a spice model of the bead and would like to simulate…
Part Number: TPS54A20 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models TI,
I'm writing because I have been working with TI-TINA models to simulate the transient behavior of the TPS54A20, the issue is that the third party…
Part Number: TPS54A20 Dear Support member,
My customer used TPS54A20.
I have two question.
Q1. Is there a calculation formula at C8 in the Data sheet Fig47? As I attaced file of question,Could you check file?
Q2. Could you tell me about the internal configuration…
Part Number: TPS54A20 Hi team,
Could you let me know the following test condition of Figure 52. Loop Response and quesion?
- injection voltage level
- recommend test condition of TPS54A20 loop response
- is Figure 52 simulation data or actual tested…