Part Number: TPS560430-Q1 I am looking for the coefficient of thermal expansion (CTE) of part numbers LMR50410YFQDBVRQ1 & TPS560430YQDBVRQ1 in the SOT-23-6 package above and below its glass transition temperature.
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Tool/software: HI Team,
Hope all is well.
My customer is Xingyu.
Currently they want to use this device for platform design, so they hope to have a standard schematic design that…
Part Number: TPS560430-Q1 Hi,
can you let me know the failure mode to be consider for TPS560430-Q1.
Also what is failure mode distribution for the above IC.
Thanks and Regards,
Mangesh
Part Number: TPS560430-Q1 Tool/software: We are usign TPS560430YQDBVRQ1 DCDC converter with input voltage of 9V to 16V and output voltage 3,3V and 0,24A output current. Fsw=2,1Meg.
We are facing an EMC problem with the NFA test (Near field antenna…
Part Number: TPS560430-Q1 Tool/software: Hi Team,
My customer Meta System is testing the unencrypted model of TPS560430-Q1, but they get below error. Can you advise how to solve?
Also, they said they need long time to stabilize the output, do you…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Tool/software: Hello,
Is it okay to use an diode at the SW in order to protect the device from Vout short to >30V?
The design is as following.
Input 12V to 16V, max load 350mA…
Part Number: TPS560430-Q1 Tool/software: 1538.5V,600mA Reg.pdf I have attached a schematic design with the input voltage of 12V and output voltage as 1.5V with the current rating of 600mA. Can anyone please confirm the design is correct or if any changes…
Part Number: TPS560430-Q1 Tool/software: Hi team,
I tested the bode plot on customer's board. It was strange.
I think it is because customer did not solder a wire on 50 ohm+. I had to link the test device to Vout pin.
Do you have a bode plot result…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Tool/software: Hello TI,
I'm using a TPS560430 and the EMI generated by switching is coupling very strongly into signal traces across my board. Each time the buck converter switches…