Part Number: TPS56121 Dear TI Support Team, We are evaluating the TPS56121DQPR and would appreciate if you could share the following data:
Efficiency derating curves or efficiency vs. load data at Ta = 125°C (and other temperatures if available).…
Part Number: TPS56121 Other Parts Discussed in Thread: TPS566238 , TPS7H4011-SP Tool/software: Dear Sir,
I'm looking for the best suitable device for a 5A constant current space laser driver, 5V to 12V input supply. Can you please advice me?
Part Number: TPS56121 Tool/software: Hi, I would like to use the TPS56121 converter as an adjustable constant current source for a nonlinear load (diode). The target parameters are: output voltage of a maximum of 8 volts, maximum current of 12 Ampere…
Part Number: TPS56121 Other Parts Discussed in Thread: LM70880-Q1 Tool/software: Hello,
I have implemented a TPS56121 circuit for a 14V input, 12V 15A output application into Pspice for TI, designed with help from Webench. Please validate the design…
Part Number: TPS56121 Regarding TPS5621 simulation, i am using Pspice-TI. I got the library on the Pspice and build the circuit.
I want to AC simulation to get the bode plot. before that i did transient one first to make sure the circuit is working…
Part Number: TPS56121
power_supply.docx
please validate attached document for fpga power supply,that sequence is ok or not and suggest us modifications
we are planning to design kintex 7 fpga based board .please suggest power supplies for that one…