Hi Zixu,
Thanks for your reply.
This is a different customer inquiry than the TPS562211/2 promotion case you mentioned. I will update you with a reply to the final email.
Regards,
JH
Hi ,
For P2P , you can refer below table.
For not p2p buck, you can try other 17v 2/3A buck : TPS563211,TPS562211,TPS563201/2/7/8,TPS562201/2/7/8.
BRs,
Young
Hi Aki,
TPS56339(SOT236 package) has high side OC protection with P2P and TPS561201. TPS563211 and TPS562211(SOT583 package) both have high side OC protection .
BRs,
Edwin.
Marco,
I would take a look at TPS562202, It doesn't have the ability to use softstart or mode selection, but I would expect it to behave similar to TPS562211.
Thanks,
Joseph
Hi,
If the Vin=5V, TPS54231 is too much over sepc as it's a 28V buck.
Are you oaky with 17V level buck? there are many options here:
TPS563211/TPS562211: 18V 2/3A buck
TPS563201/2 : 17V 3A buck
TPS562201/2: 17V 2A buck
TPS563231: 17V 3A buck
and if…
Hi Denny,
For the min duty support, suggest to consider the worst case Duty=110 ns* Max Freq 510 Khz = 5.6% .
For 18Vin-0.8Vout , 2/3A solution , suggest to choose TPS56339 (24Vin 3A SOT236) or TPS563211 (18Vin,3A, SOT583) ,TPS562211 (18Vin ,2A,SOT583…
Other Parts Discussed in Thread: TPS563210A , TPS563219A , TPS562219A , TPS562210A , TPS562211 , TPS563211 Are there P2P compatible parts for TPS562219ADDFR?
Hi,
Think TPS563211, tps562211 , 4.2V-18V , 3A/2A devices , are good for your application . They are all APLed , will RTM in Sep'21. Mode pin can be used to configure ECO/FCCM+PG/SS .
if lower Vin is acceptable , TPS563201/2/7/8 and TPS562201/2/7…
Other Parts Discussed in Thread: TPS563211 , TPS562211 , TPS563201 , TPS56339 Hi team,
Could you help recommend a module or buck converter IC which height is lower than 1.2mm ?
The spec requirement is below.
4.5V~18V in/ 3.3V 0.5A out
Thanks!