Part Number: TPS563209 Other Parts Discussed in Thread: TINA-TI Hi, Customers are trying to make inversion circuits using TPS563209. Is it possible to realize an inverting circuit using this device? Customers are considering circuits like the following materials…
Part Number: TPS563209 Dear TI'er.
below show TPS563209 circuit. Vin = 12V , Vout = 5V
When power on, Vout waveform has drop ( about 12ms ) . Please help to check what's happen.
Part Number: TPS563209 Hi,
We got a question from customer about TPS563209. Could you help us?
[Question] There is Iout vs Ta characteristics in datasheet figure 16. What does the line represent on this figure? Why does the output current be reduced in high…
Part Number: TPS563209 Hi,
I found the current limit spec at TPS563209 datasheet as below.
And the condition is Vout=1.05V, but I need the Iocl spec at VOUT=5V.
Can you share the CURRENT LIMIT spec at VOUT=5V?
thanks,
TS
Other Parts Discussed in Thread: TPS563209 Dear TI employee.
Do you kwon which FeedBack resistor value as shown blow.
I know recommmend resistor value(33.2KOhm, 10KOhm) in datasheet for 3.3v output .
Can I use 332 Ohm, 100 Ohm feedback resistor for 3…
Other Parts Discussed in Thread: TPS563209 Hi, Could you tell me about EN pull up resistor? Would you need this? I would like to know the reason for pull up registor. Best Regards, Yusuke/Japan Disty
Hi
I want to know exactly.
What are the efficiencies? when is Input Voltage: 12V and Output Voltage: 1.0V, Current Load: 2.6A?
There are't expressed in datasheet as shown below
If you have any question. Anytime contact me.
Other Parts Discussed in Thread: TPS563209 Hello, TI employee.
I had been use TPS563209 for Broadcom Core Voltage
TPS563209 Input: 12V, Output: 1.0V, Broadcom Current(BCM7584 Current normal: 2.4A Max: 2.6A, BCM7583 Current normal: 1.4A MAX: 1.7A)
I took…
Other Parts Discussed in Thread: TPS563209 , TPS54327 Hello
The results were attached document I simulated thermal characteristics of TPS563209 and TPS54327 by WEBENCH. Pd of TPS563209 grows big with a rise in temperature, but TPS54327 is uniform regardless…
Hi, Could you tell me about TPS56X209 FB voltage accuracy in Tj=-40℃ to 150℃? Customer use temperature range is wide. Therefore the customer wants to know it. Best Regards, Yusuke/Japan Disty