Part Number: TPS563219A Hello team,
The pin assignments in the TPS563219 data sheet differ between P.3 (Pin Configuration and Functions) and P.21 (Layout Example). Which should I refer to?
The positions of the PG pin and SS pin were reversed in the layout…
Part Number: TPS563219A Tool/software: WEBENCH® Design Tools In following condition
Vin=6.2V, Vo=5.0V, Io=1.5A
Design can not be create by webench.Please let us know the reason.
Part Number: TPS563219A
Hello,
Datasheet 7.3.4 says “And then, the device will shut down after the UVP delay time (typically 14 μs) and re-start after the hiccup time.” Here, the hiccup time means tHiccupOn specified in 6.5?
…
Part Number: TPS563219A Dear Team,
As you can see after the converter's output, the customer already implements lots of filters to reduce the ripple.
But the customer's target is under 3.5mV at VCC_C_PLL_AVDD1P, do you have any suggestions?
The…
Part Number: TPS563219A It seems to regulate voltage at VFB to approx 1.4V. Using eq.2 and fig.17 I cannot set output voltage to 2V using R1 = 16.1k and R2 = 10k. This setting results in VOUT=4V.
Part Number: TPS563219A Hello,
Our customer asked bout if TPS563219A has output discharge function when it is disabled, because his application required strict power down sequence.
Best regards,
Part Number: TPS563219A Hello,
Would you please check layout of GND pattern below
IC701 is TPS563219A.
Is it okay below layout?
- GND pattern layout under the device and connects GND for VIN and VOUT.
- There is via hole under the device which connects…